Skip to main content
Associate
May 23, 2025
Question

STM32CubeMX HAL generated code for STM32F051 faulty

I'm using STM32CubeMX 6.14.1
Recently I was added DAC to my project. I doesn't suppose to use DAC with interrupt, I wasn't enable it, but occasionally I was enabled DAC callbacks.
Generated the code for Makefile based project.
In the end of building process, linker thrown errors:

/usr/lib/gcc/arm-none-eabi/12.2.1/../../../arm-none-eabi/bin/ld: build/stm32f0xx_hal_dac.o: in function `HAL_DAC_Init':
/home/tovis/nusi/worke/STM32/F051_ccl/Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_dac.c:304: undefined reference to `HAL_DACEx_ConvCpltCallbackCh2'
/usr/lib/gcc/arm-none-eabi/12.2.1/../../../arm-none-eabi/bin/ld: /home/tovis/nusi/worke/STM32/F051_ccl/Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_dac.c:304: undefined reference to `HAL_DACEx_ConvHalfCpltCallbackCh2'
/usr/lib/gcc/arm-none-eabi/12.2.1/../../../arm-none-eabi/bin/ld: /home/tovis/nusi/worke/STM32/F051_ccl/Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_dac.c:304: undefined reference to `HAL_DACEx_ErrorCallbackCh2'

I made some investigation, and turns out, that in generated code stm32f0xx_hal_dac.c DAC handled as it have two channel - STN32F051 have only one channel DAC. From the other side, where the callbacks are defined there is a series #ifdef and list of STM32F0xx MCUs which have two channel DAC (stm32f0xx_hal_dac_ex.c row: 1088). With this setup callbacks for the second channel aren't generated, what leads to linker error.

When I understand what's the problem, I simply disabled callbacks. My problem is solved, but I think it's a bug and sometime shall be corrected.

This topic has been closed for replies.

5 replies

STTwo-32
ST Technical Moderator
May 23, 2025

Hello @tovis 

could you please upload your .ioc file.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
tovisAuthor
Associate
May 24, 2025

Thank you for quick respond.
In the attached .ioc file the DAC callbacks are disabled.

To reproduce the problem, you should enable DAC callbacks.