Skip to main content
leshich-k
Associate II
Feb 10, 2020 1:17 PM UTC
Question

STM32CubeMX H7 PTP not supported by MAC Ethernet Driver

Up till now (v1.6.0) there is no support for PTP in MAC Ethernet driver. WHen will it be added?

This topic has been closed for replies.

3 replies

Piranha
Principal III
Feb 10, 2020 11:18 PM UTC

Better worry about the fact that H7 driver is not working at all...

https://community.st.com/s/question/0D50X0000BOtfhnSQB/how-to-make-ethernet-and-lwip-working-on-stm32

As for PTP - it's a pretty simple (part of) peripheral. It's hard to even imagine what a PTP "driver" should do. Write few integer values into registers through one line long functions like in LL "drivers"?

leshich-k
leshich-kAuthor
Associate II
Feb 11, 2020 10:37 AM UTC

Pretty simple, that's why I wander why is it not realized yet?

Up till now I was working on F7 series, and now our company desided to move to H7.

Not working at all? What I see is that RX and TX frames are getting transferred well. LwIP is going to be the next step to run.