Skip to main content
TThan
Associate III
February 12, 2026
Solved

STM32CubeMX generated USBPD not compiling

Hello,

I created a complex project for a STM32H573 based custom board. That project is ThreadX based and it shall use the USPBD package.

I generated to project with STM32CubeMX version 6.16.1 using STM32Cube MCU Package for STM32H5 Series 1.5.1 (see attached IOC file for reference)

I create the code for the latest STM32CubeIDE 2.0.0. The project is imported successfully, but does not compile and the following errors are logged:

Description	Resource	Path	Location	Type
'USBPD_CORE_PDO_TYPE_APDO' undeclared (first use in this function); did you mean 'USBPD_CORE_PDO_TYPE_FIXED'?	usbpd_dpm_user.c	/test03/USBPD/Target	line 1100	C/C++ Problem
'USBPD_CORE_PDO_TYPE_APDO' undeclared (first use in this function); did you mean 'USBPD_CORE_PDO_TYPE_FIXED'?	usbpd_dpm_user.c	/test03/USBPD/Target	line 1577	C/C++ Problem
'USBPD_ParamsTypeDef' has no member named 'PE_UnchunkSupport'	usbpd_dpm_user.c	/test03/USBPD/Target	line 1507	C/C++ Problem
'USBPD_ParamsTypeDef' has no member named 'PE_UnchunkSupport'	usbpd_dpm_user.c	/test03/USBPD/Target	line 1511	C/C++ Problem
'USBPD_PDO_TypeDef' has no member named 'SRCSNKAPDO'	usbpd_dpm_user.c	/test03/USBPD/Target	line 1275	C/C++ Problem
'USBPD_PDO_TypeDef' has no member named 'SRCSNKAPDO'	usbpd_dpm_user.c	/test03/USBPD/Target	line 1276	C/C++ Problem
'USBPD_PDO_TypeDef' has no member named 'SRCSNKAPDO'	usbpd_dpm_user.c	/test03/USBPD/Target	line 1295	C/C++ Problem
'USBPD_PDO_TypeDef' has no member named 'SRCSNKAPDO'	usbpd_dpm_user.c	/test03/USBPD/Target	line 1296	C/C++ Problem
'USBPD_PDO_TypeDef' has no member named 'SRCSNKAPDO'	usbpd_dpm_user.c	/test03/USBPD/Target	line 1297	C/C++ Problem
make: *** [USBPD/App/subdir.mk:28: USBPD/App/usbpd_dpm_core.o] Error 1	test03		 	C/C++ Problem
make: *** [USBPD/App/subdir.mk:28: USBPD/App/usbpd_pwr_if.o] Error 1	test03		 	C/C++ Problem
make: *** [USBPD/App/subdir.mk:28: USBPD/App/usbpd.o] Error 1	test03		 	C/C++ Problem
make: *** [USBPD/Target/subdir.mk:22: USBPD/Target/usbpd_dpm_user.o] Error 1	test03		 	C/C++ Problem
make: *** Waiting for unfinished jobs....	test03		 	C/C++ Problem
unknown type name 'USBPD_PPSSDB_TypeDef'	usbpd_dpm_user.h	/test03/USBPD/Target	line 96	C/C++ Problem

When looking at the code, I do not understand why these defines and types are missing, they should all be there.It looks like there are some project settings missing or wrong set. Maybe there is a bug in the code generator?

Any help on getting this to compile would be highly appreciated.

Thank you!
/Thomas

ST Technical Moderator
February 17, 2026

Hello @TThan,

 

After investigating internally, the configuration of USBPD should be changed from [Min Sink] to [Full Stack].

Only [Full stack] option could be selected, and the other options will be grayed out when X-Cube-TCPP is enabled.

MahmoudBenRomdhane_1-1771340919066.png

 

Thanks.

Mahmoud

 

 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

ST Technical Moderator
February 12, 2026

Hello@TThan

Let me thank you for your post.

I am currently checking this behavior, and I will get back to you ASAP.

Thanks

Mahmoud 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Technical Moderator
February 16, 2026

Hello @TThan 

 

Let me thank for bringing this issue to our attention.

The issue has been escalated internally to the dedicated team for further investigation and resolution (Ticket 227242).

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
TThan
TThanAuthor
Associate III
February 16, 2026

Hello Mahmoud,

thank you for investigating on this.

/Thomas