Skip to main content
Associate
February 5, 2026
Solved

[STM32CubeMX Feature request] STM32CubeMX RAM/FLASH UI memory map improvements

  • February 5, 2026
  • 2 replies
  • 275 views

Hi everyone,

I'm currently porting the App of STM32U5 SBSFU example to CubeMX and "smooth" is not the word I would use to describe the process.

Namely, the SBSFU example includes Bootloader, Loader and App projects with memory map being in separate centralized header files included by all these projects. These files (region_defs and flash_layout) are not fully polished (some bugginess and inconsistencies) but they do ease the memory management a lot by using defines and not hardcoding; these defines are then used in projects' linker files in order to define memory regions.

In contrast, CubeMX just provides a UI representation of the memory space where users can input all the memory bounds, be it flash or RAM. The trouble is, we can only enter numbers and not constants, so generated code is full of hardcoded address bounds.

This does not play well with SBSFU Example - since these address bounds are not only used in LD files, but rather for defining FLASH areas, SAU regions etc etc, it is an enormous amount of work to get this synchronized.

My suggestion that would dramatically improve productivity here:

Add support for using constants in UI memory map tool in CubeMX: since we can even set these constants in CubeMX, you could even implement a sanity check when generating. Although I've already seen that sanity checks are not a strong side of CubeMX (e.g. unbuildable projects are generated out-of-the-box), at least for trustzone Apps, there are ALWAYS changes needed to BSP after the generation, which implies users are already used to this and are expecting it :)

Anyway, would love to know if anyone has similar issues as well and finds this a good idea?

Cheers!

Ivan

Best answer by Ghofrane GSOURI

Hello @ikozic 

Your contribution is greatly appreciated.

Your change request has been forwarded to the development team under internal ticket ID 227180 for further assessment and feasibility analysis.

I will keep you informed of any update

THX

Ghofrane

2 replies

Ghofrane GSOURI
ST Technical Moderator
February 5, 2026

Hello @ikozic 

I'm currently checking your request. I will get back to you asap.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
February 13, 2026

Hello @ikozic 

Your contribution is greatly appreciated.

Your change request has been forwarded to the development team under internal ticket ID 227180 for further assessment and feasibility analysis.

I will keep you informed of any update

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.