Skip to main content
BHans
Associate
Mar 22, 2019 3:15 PM UTC
Question

STM32CubeMX - Conflicting Generated Function Call Ranks

I have a fairly simple project defined in CubeMX based on one of the H7-series of STM32 parts. This project utilizes a number of peripherals and DMA channels, including the MDMA and RTC peripherals.

As I configured an additional DMA channel for a USART, CubeMX seemed to "break down" at this, and began overlapping several function calls when they were generated. It also began to leave one call in main() out each time I regenerated code. Upon further inspection, I realized that each time I save my project, even without any changes to my project settings, I can cause CubeMX to reorder the items in the "Project Manager"->"Advanced Settings" page. Additionally, it doesn't contain a "3" rank item, and it continually swaps between showing any two of the "MX_DMA_Init", "MX_MDMA_Init", or "MX_RTC_Init" functions.

It's extremely bizarre behavior, and it's giving me far less confidence in my generated code if there's weird faults going on during the process that are seemingly uncontrollable by myself.

Has anyone experienced this before, and might be able to shed some light on what I'm doing wrong?

This topic has been closed for replies.

5 replies

Khouloud ZEMMELI
ST Employee
Mar 22, 2019 3:18 PM UTC

​hello @BHans​ 

Thank you for the feedback,

This is reported internally for further check.

Best Regards,

Khouloud.

Khouloud ZEMMELI
ST Employee
Mar 22, 2019 3:23 PM UTC

@BHans​  could you please share your ioc file?

Khouloud.​

BHans
BHansAuthor
Associate
Mar 22, 2019 3:28 PM UTC

Do you have a method by which I can upload directly to you instead of to a public forum? I cannot share this .ioc publicly.

Khouloud ZEMMELI
ST Employee
Mar 22, 2019 3:32 PM UTC

@BHans​ 

you can send it as a private message.

Khouloud

Khouloud ZEMMELI
ST Employee
Mar 22, 2019 3:58 PM UTC

​@BHans​ 

You are right, issue will be fixed in the next release.

Best Regards,

Khouloud.