Skip to main content
sasha
Associate III
Feb 13, 2018 10:38 PM UTC
Question

STM32CubeMX build problems when 'build under root' is selected with TrueStudio

Posted on February 13, 2018 at 23:38

Hi There,

I've just switched to using Atollic (from System Workbench) and am having issues with the code generation in STM32CubeMX.  When I build a project using 'generate under root', the code will not compile with undefined references to all the HAL functions.

e.g. errors like

..\STM32_workspace_9.0\TEST_PROJECT_UNDERROOT\Debug/..\Src/hrtim.c:69: undefined reference to `HAL_HRTIM_Init'

If I generate with this box unticked then there are no problems.

I am using:

STM32CubeMX V4.24

STM32Cube FW_F3 V1.9.0

Atollic TrueStudio V9.0.0

#atollic-truestudio #stm32cubemx
This topic has been closed for replies.

2 replies

ST Technical Moderator
Feb 14, 2018 1:40 PM UTC
Posted on February 14, 2018 at 14:40

Hello ,

Please check if you have the same issue with CubeMx version 4.24 reported in this discussion

https://community.st.com/0D50X00009XkWopSAF

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Houda GHABRI
ST Employee
Apr 11, 2018 1:31 PM UTC
Posted on April 11, 2018 at 15:31

Hello Marks,

thanks for your feedback.

I'm not able to reproduce the problem.

could you please give me more details about the scenario to reproduce it or send me the ioc?

best regards,

Houda