Skip to main content
greg2399
Visitor II
Aug 24, 2015 8:08 PM UTC
Question

STM32CubeMX Bug: NbrOfDiscConversion not set

Posted on August 24, 2015 at 22:08

When Discontinuous Conversion Mode is disabled CubeMX leaves the NbrOfDiscConversion field in ADC_InitTypeDef uninitialized which can cause assert_param(IS_ADC_REGULAR_NB_CONV(hadc->Init.NbrOfConversion)) in 

HAL_ADC_Init to trigger resulting in an assert failure.

CubeMx Version 4.9.0

STM32Cube FW_L1 V1.3.0

#bug #stm32cubemx #stm32l #assert
This topic has been closed for replies.

2 replies

stm32cube-t
ST Employee
Aug 26, 2015 2:41 PM UTC
Posted on August 26, 2015 at 16:41

Dear user,

thank you for reporting this issue.

Actually, the parameter

NbrOfDiscConversion

shall not be initialized when Discontinuous conversion is disabled.

The ADC HAL driver will be corrected so that the following line is executed only if Discontinuous conversion is enabled:

assert_param(IS_ADC_REGULAR_DISCONT_NUMBER(hadc->Init.NbrOfDiscConversion));

Best regards
stm32cube-t
ST Employee
Oct 12, 2015 8:46 AM UTC
Posted on October 12, 2015 at 10:46

Dear user,

The fix will be delivered within STM32L1 1.4.0 package supported in our next CubeMX version 4.11 (coming out this month).

Thanks.