Hello @SamVDA
STM32CubeMX 6.16.0 and MX 6.16.1 are supported on
• Windows® 10 32 bits (x86) or 64 bits (x64), and Windows® 11 64 bits (x64)
• Linux®: Ubuntu® LTS 22.04 and LTS 24.04, and Fedora® 42
• macOS® 15 (Sequoia), macOS® 26 (Tahoe): x86_64 and ARM-aarch64 architectures
Since your operating system is Windows 11, STM32CubeMX should work correctly on your machine.
If there is any issue, it should normally be reported in the log files. As the logs do not show any critical errors, the problem is likely related to your local environment.
Let's try to uninstall STM32CubeMX and reinstall it again.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.