Skip to main content
asrock70
Associate III
January 3, 2015
Question

STM32CubeMX and F1 package v1.3

Posted on January 03, 2016 at 13:40

I have STM32CubeMX v4.12, Check for Updates

revealed

STM32CubeF1 Release 1.3

After dondloadint , but Cube say:

This Package version is not managed on this version of STM32CubeMX.

Wher is probl�m?

 

I am talking

about

 

http://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF260820?s_searchtype=keyword

#stm32cube #stm32cubemx #stm32f1
This topic has been closed for replies.

6 replies

Nesrine M_O
Associate
January 4, 2016
Posted on January 04, 2016 at 11:53

Hi Charles,

Could you please explain how you get the firmware update: is it automatically asked by MX or did you selected a local installation done manually?

-Syrine-

asrock70
asrock70Author
Associate III
January 4, 2016
Posted on January 04, 2016 at 18:14

For the first time

offered

me the

MX

update

automatically

over Check update Manager

After the failure

, I

tried

and manual

installation.

For completeness

,

the MX

now

has

this update

no

offers

.

asrock70
asrock70Author
Associate III
January 5, 2016
Posted on January 05, 2016 at 09:23

Type text or a website address or

https://translate.google.cz/?tr=f&hl=en

https://translate.google.cz/?tr=t&hl=en

</div>

Translate from:

Yesterday I

discovered the

STM32Cube

F1 1.3

 

updates

on the second

PC.

Downloading and installing

OK

.

In New Libraries Manager I see STM32Cube F1 Releases 1.2 and 1.3 too, all with green square as installed.

After restarting STM32CubeMX, I see only version 1.2, Check Update Manager not offer any update. In folder Repository is folder STM32Cube_FW_F1_V1.2.0 and

STM32Cube_FW_F1_V1.3.0 too.

OS I have Windows 7 x64 on first PC and Windows 7 x86 on second PC, all updates Installed.

Installation MX is standard only, installation folder changed from C:\.. to D:\..  and Repository Folder changed on D:\Program Files\STMicroelectronics\STM32Cube\Repository

astrid
Associate II
January 10, 2016
Posted on January 10, 2016 at 12:33

I today on new computer install last version of CubeMX 4.12.

Unfortunately,

it

also

offered as

the latest version

CubeF1

v 1.2

Version

1.3

can not be installed

for manual

download from the

ST web page.
edelmann
Associate II
January 15, 2016
Posted on January 15, 2016 at 12:41

Dear Sir/Madam,

I can confirm the issue as experienced on my PC.

Latest STM32CubeMX has been installed (V4.12.0),

Installation of STM32Cube_FW_F1_V1.3.0 from local download fails with error message: ''This Package version is not managed on this version of STM32CubeMX.''

Due to firewall restrictions, direct update download could not be tested.

Best regards

Nesrine M_O
Associate
January 20, 2016
Posted on January 20, 2016 at 11:56

Hi,

The STM32CubeF1 Firmware Package V1.3.0 is now available for download using update interface of MX 4.12.

-Syrine-