Skip to main content
FPlow.1
Associate
February 10, 2023
Solved

STM32CubeMX 6.7.0 does not configure SDMMC DMA correctly

I am having an issue similar to https://community.st.com/s/question/0D53W000027iXpbSAE/spi-dma-configuration-generated-by-stm32cubemx-does-not-work but with the SDMMC peripheral rather than SPI.

I have an STM32CubeMX project targeting the 32F746GDISCOVERY with the following relevant peripherals and settings:

  • SDMMC SD 4 Bits Wide bus
    • SDMMC1 global interrupt enabled
    • SDMMC1 bidirectional DMA request enabled on DMA2 stream 3
  • FatFS enabled with DMA template

With the above STM32CubeMX configuration and the minimum working example below:

#define TEST_DATA_SIZE 32768
 
// -- snip
 
static FRESULT fatfs_err;
static const unsigned char test_data[TEST_DATA_SIZE] __attribute__ ((section (".dtcm"), aligned (4))) = {0};
static unsigned int bytes;
 
// -- snip
 
int main(void) {
 // -- snip
 
 fatfs_err = f_mount(&SDFatFS, SDPath, 1);
 if (fatfs_err != FR_OK) {
 printf("failed to mount card, code: %i.\n", fatfs_err);
 if (fatfs_err != FR_NOT_READY) {
 printf("exiting.\n");
 exit(fatfs_err);
 }
 printf("continuing.\n");
 }
 
 // Open file
 fatfs_err = f_open(&SDFile, "test.txt", FA_WRITE | FA_CREATE_ALWAYS);
 if (fatfs_err != FR_OK) {
 printf("failed to open file, code: %i.\n", fatfs_err);
 printf("exiting.\n");
 exit(fatfs_err);
 }
 
 // Write file
 fatfs_err = f_write(&SDFile,
 test_data,
 TEST_DATA_SIZE,
 &bytes);
 if (fatfs_err != FR_OK) {
 printf("failed to write file, code: %i\n", fatfs_err);
 printf("exiting.\n");
 exit(fatfs_err);
 }
 if (bytes != TEST_DATA_SIZE) {
 printf("wrote %i bytes, less than the expected %i.\n",
 bytes, TEST_DATA_SIZE);
 }
 
 // Close file
 fatfs_err = f_close(&SDFile);
 if (fatfs_err != FR_OK) {
 exit(fatfs_err);
 }
 
 // -- snip

The project works fine on 6.6.1, but as soon as I migrate to 6.7.0 the SDMMC peripheral times out. Specifically, it hangs on line 220 of sd_diskio.c, while waiting for a DMA callback.

This topic has been closed for replies.
FPlow.1
FPlow.1Best answer
Associate
February 10, 2023

Where 661 and 670 are STM32CubeIDE projects generated by STM32CubeMX 6.6.1 and 6.7.0, respectively, this command:

diff -r 661 670 --exclude ".project" --exclude ".cproject" --exclude ".settings" --exclude "Debug"

produces the following output

Only in 661: 661 Debug.launch
Only in 661: 661.ioc
Only in 670: 670 Debug.launch
Only in 670: 670.ioc
diff -r --ex 661/Core/Inc/main.h 670/Core/Inc/main.h
383a384
> 
diff -r --ex 661/Core/Inc/stm32f7xx_hal_conf.h 670/Core/Inc/stm32f7xx_hal_conf.h
40,62c40,61
< /* #define HAL_ADC_MODULE_ENABLED */
< /* #define HAL_CRYP_MODULE_ENABLED */
< /* #define HAL_CAN_MODULE_ENABLED */
< /* #define HAL_CEC_MODULE_ENABLED */
< /* #define HAL_CRC_MODULE_ENABLED */
< /* #define HAL_CRYP_MODULE_ENABLED */
< /* #define HAL_DAC_MODULE_ENABLED */
< /* #define HAL_DCMI_MODULE_ENABLED */
< /* #define HAL_DMA2D_MODULE_ENABLED */
< /* #define HAL_ETH_MODULE_ENABLED */
< /* #define HAL_NAND_MODULE_ENABLED */
< /* #define HAL_NOR_MODULE_ENABLED */
< /* #define HAL_SRAM_MODULE_ENABLED */
< /* #define HAL_SDRAM_MODULE_ENABLED */
< /* #define HAL_HASH_MODULE_ENABLED */
< /* #define HAL_I2S_MODULE_ENABLED */
< /* #define HAL_IWDG_MODULE_ENABLED */
< /* #define HAL_LPTIM_MODULE_ENABLED */
< /* #define HAL_LTDC_MODULE_ENABLED */
< /* #define HAL_QSPI_MODULE_ENABLED */
< /* #define HAL_RNG_MODULE_ENABLED */
< /* #define HAL_RTC_MODULE_ENABLED */
< /* #define HAL_SAI_MODULE_ENABLED */
---
> /* #define HAL_CRYP_MODULE_ENABLED */
> /* #define HAL_ADC_MODULE_ENABLED */
> /* #define HAL_CAN_MODULE_ENABLED */
> /* #define HAL_CEC_MODULE_ENABLED */
> /* #define HAL_CRC_MODULE_ENABLED */
> /* #define HAL_DAC_MODULE_ENABLED */
> /* #define HAL_DCMI_MODULE_ENABLED */
> /* #define HAL_DMA2D_MODULE_ENABLED */
> /* #define HAL_ETH_MODULE_ENABLED */
> /* #define HAL_NAND_MODULE_ENABLED */
> /* #define HAL_NOR_MODULE_ENABLED */
> /* #define HAL_SRAM_MODULE_ENABLED */
> /* #define HAL_SDRAM_MODULE_ENABLED */
> /* #define HAL_HASH_MODULE_ENABLED */
> /* #define HAL_I2S_MODULE_ENABLED */
> /* #define HAL_IWDG_MODULE_ENABLED */
> /* #define HAL_LPTIM_MODULE_ENABLED */
> /* #define HAL_LTDC_MODULE_ENABLED */
> /* #define HAL_QSPI_MODULE_ENABLED */
> /* #define HAL_RNG_MODULE_ENABLED */
> /* #define HAL_RTC_MODULE_ENABLED */
> /* #define HAL_SAI_MODULE_ENABLED */
64,80c63,79
< /* #define HAL_MMC_MODULE_ENABLED */
< /* #define HAL_SPDIFRX_MODULE_ENABLED */
< /* #define HAL_SPI_MODULE_ENABLED */
< /* #define HAL_TIM_MODULE_ENABLED */
< /* #define HAL_UART_MODULE_ENABLED */
< /* #define HAL_USART_MODULE_ENABLED */
< /* #define HAL_IRDA_MODULE_ENABLED */
< /* #define HAL_SMARTCARD_MODULE_ENABLED */
< /* #define HAL_WWDG_MODULE_ENABLED */
< /* #define HAL_PCD_MODULE_ENABLED */
< /* #define HAL_HCD_MODULE_ENABLED */
< /* #define HAL_DFSDM_MODULE_ENABLED */
< /* #define HAL_DSI_MODULE_ENABLED */
< /* #define HAL_JPEG_MODULE_ENABLED */
< /* #define HAL_MDIOS_MODULE_ENABLED */
< /* #define HAL_SMBUS_MODULE_ENABLED */
< /* #define HAL_EXTI_MODULE_ENABLED */
---
> /* #define HAL_MMC_MODULE_ENABLED */
> /* #define HAL_SPDIFRX_MODULE_ENABLED */
> /* #define HAL_SPI_MODULE_ENABLED */
> /* #define HAL_TIM_MODULE_ENABLED */
> /* #define HAL_UART_MODULE_ENABLED */
> /* #define HAL_USART_MODULE_ENABLED */
> /* #define HAL_IRDA_MODULE_ENABLED */
> /* #define HAL_SMARTCARD_MODULE_ENABLED */
> /* #define HAL_WWDG_MODULE_ENABLED */
> /* #define HAL_PCD_MODULE_ENABLED */
> /* #define HAL_HCD_MODULE_ENABLED */
> /* #define HAL_DFSDM_MODULE_ENABLED */
> /* #define HAL_DSI_MODULE_ENABLED */
> /* #define HAL_JPEG_MODULE_ENABLED */
> /* #define HAL_MDIOS_MODULE_ENABLED */
> /* #define HAL_SMBUS_MODULE_ENABLED */
> /* #define HAL_EXTI_MODULE_ENABLED */
213c212
< #define ETH_RX_BUF_SIZE ETH_MAX_PACKET_SIZE /* buffer size for receive */
---
> #define ETH_RX_BUF_SIZE /* buffer size for receive */
diff -r --ex 661/Core/Src/main.c 670/Core/Src/main.c
218c218
< hsd1.Init.BusWide = SDMMC_BUS_WIDE_1B;
---
> hsd1.Init.BusWide = SDMMC_BUS_WIDE_4B;
diff -r --ex 661/Core/Src/syscalls.c 670/Core/Src/syscalls.c
13c13
< * Copyright (c) 2022 STMicroelectronics.
---
> * Copyright (c) 2020-2022 STMicroelectronics.
50c50
< 	return 1;
---
> return 1;
55,56c55,58
< 	errno = EINVAL;
< 	return -1;
---
> (void)pid;
> (void)sig;
> errno = EINVAL;
> return -1;
61,62c63,64
< 	_kill(status, -1);
< 	while (1) {}		/* Make sure we hang here */
---
> _kill(status, -1);
> while (1) {} /* Make sure we hang here */
67c69,70
< 	int DataIdx;
---
> (void)file;
> int DataIdx;
69,72c72,75
< 	for (DataIdx = 0; DataIdx < len; DataIdx++)
< 	{
< 		*ptr++ = __io_getchar();
< 	}
---
> for (DataIdx = 0; DataIdx < len; DataIdx++)
> {
> *ptr++ = __io_getchar();
> }
74c77
< return len;
---
> return len;
79c82,83
< 	int DataIdx;
---
> (void)file;
> int DataIdx;
81,85c85,89
< 	for (DataIdx = 0; DataIdx < len; DataIdx++)
< 	{
< 		__io_putchar(*ptr++);
< 	}
< 	return len;
---
> for (DataIdx = 0; DataIdx < len; DataIdx++)
> {
> __io_putchar(*ptr++);
> }
> return len;
90c94,95
< 	return -1;
---
> (void)file;
> return -1;
96,97c101,103
< 	st->st_mode = S_IFCHR;
< 	return 0;
---
> (void)file;
> st->st_mode = S_IFCHR;
> return 0;
102c108,109
< 	return 1;
---
> (void)file;
> return 1;
107c114,117
< 	return 0;
---
> (void)file;
> (void)ptr;
> (void)dir;
> return 0;
112,113c122,125
< 	/* Pretend like we always fail */
< 	return -1;
---
> (void)path;
> (void)flags;
> /* Pretend like we always fail */
> return -1;
118,119c130,132
< 	errno = ECHILD;
< 	return -1;
---
> (void)status;
> errno = ECHILD;
> return -1;
124,125c137,139
< 	errno = ENOENT;
< 	return -1;
---
> (void)name;
> errno = ENOENT;
> return -1;
130c144,145
< 	return -1;
---
> (void)buf;
> return -1;
135,136c150,152
< 	st->st_mode = S_IFCHR;
< 	return 0;
---
> (void)file;
> st->st_mode = S_IFCHR;
> return 0;
141,142c157,160
< 	errno = EMLINK;
< 	return -1;
---
> (void)old;
> (void)new;
> errno = EMLINK;
> return -1;
147,148c165,166
< 	errno = EAGAIN;
< 	return -1;
---
> errno = EAGAIN;
> return -1;
153,154c171,175
< 	errno = ENOMEM;
< 	return -1;
---
> (void)name;
> (void)argv;
> (void)env;
> errno = ENOMEM;
> return -1;

Based on this, I tried changing

hsd1.Init.BusWide = SDMMC_BUS_WIDE_4B;

to

hsd1.Init.BusWide = SDMMC_BUS_WIDE_1B;

in the 6.7.0 project and it fixed the issue. Note this is not the same as running the card in 1-bit mode, the FatFS Disk I/O driver switches it to 4-bit mode later in initialisation:

~/SDMMC_STM32CubeMX_Test/661 % rg "SDMMC_BUS_WIDE_4B"
Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_sd.c
2180: * @arg SDMMC_BUS_WIDE_4B: 4-bit data transfer
2202: else if(WideMode == SDMMC_BUS_WIDE_4B)
 
Drivers/STM32F7xx_HAL_Driver/Inc/stm32f7xx_ll_sdmmc.h
365:#define SDMMC_BUS_WIDE_4B SDMMC_CLKCR_WIDBUS_0
369: ((WIDE) == SDMMC_BUS_WIDE_4B) || \
 
Debug/661.list
10552: * @arg SDMMC_BUS_WIDE_4B: 4-bit data transfer
10597: else if(WideMode == SDMMC_BUS_WIDE_4B)
14765: if (HAL_SD_ConfigWideBusOperation(&hsd1, SDMMC_BUS_WIDE_4B) != HAL_OK)
 
FATFS/Target/bsp_driver_sd.c
62: if (HAL_SD_ConfigWideBusOperation(&hsd1, SDMMC_BUS_WIDE_4B) != HAL_OK)

I'm not quite sure what the whole sequence is for initialisation in the SD specification, but I think the card has to be in 1-bit mode first in order to set up 4-bit mode.

2 replies

FPlow.1
FPlow.1AuthorBest answer
Associate
February 10, 2023

Where 661 and 670 are STM32CubeIDE projects generated by STM32CubeMX 6.6.1 and 6.7.0, respectively, this command:

diff -r 661 670 --exclude ".project" --exclude ".cproject" --exclude ".settings" --exclude "Debug"

produces the following output

Only in 661: 661 Debug.launch
Only in 661: 661.ioc
Only in 670: 670 Debug.launch
Only in 670: 670.ioc
diff -r --ex 661/Core/Inc/main.h 670/Core/Inc/main.h
383a384
> 
diff -r --ex 661/Core/Inc/stm32f7xx_hal_conf.h 670/Core/Inc/stm32f7xx_hal_conf.h
40,62c40,61
< /* #define HAL_ADC_MODULE_ENABLED */
< /* #define HAL_CRYP_MODULE_ENABLED */
< /* #define HAL_CAN_MODULE_ENABLED */
< /* #define HAL_CEC_MODULE_ENABLED */
< /* #define HAL_CRC_MODULE_ENABLED */
< /* #define HAL_CRYP_MODULE_ENABLED */
< /* #define HAL_DAC_MODULE_ENABLED */
< /* #define HAL_DCMI_MODULE_ENABLED */
< /* #define HAL_DMA2D_MODULE_ENABLED */
< /* #define HAL_ETH_MODULE_ENABLED */
< /* #define HAL_NAND_MODULE_ENABLED */
< /* #define HAL_NOR_MODULE_ENABLED */
< /* #define HAL_SRAM_MODULE_ENABLED */
< /* #define HAL_SDRAM_MODULE_ENABLED */
< /* #define HAL_HASH_MODULE_ENABLED */
< /* #define HAL_I2S_MODULE_ENABLED */
< /* #define HAL_IWDG_MODULE_ENABLED */
< /* #define HAL_LPTIM_MODULE_ENABLED */
< /* #define HAL_LTDC_MODULE_ENABLED */
< /* #define HAL_QSPI_MODULE_ENABLED */
< /* #define HAL_RNG_MODULE_ENABLED */
< /* #define HAL_RTC_MODULE_ENABLED */
< /* #define HAL_SAI_MODULE_ENABLED */
---
> /* #define HAL_CRYP_MODULE_ENABLED */
> /* #define HAL_ADC_MODULE_ENABLED */
> /* #define HAL_CAN_MODULE_ENABLED */
> /* #define HAL_CEC_MODULE_ENABLED */
> /* #define HAL_CRC_MODULE_ENABLED */
> /* #define HAL_DAC_MODULE_ENABLED */
> /* #define HAL_DCMI_MODULE_ENABLED */
> /* #define HAL_DMA2D_MODULE_ENABLED */
> /* #define HAL_ETH_MODULE_ENABLED */
> /* #define HAL_NAND_MODULE_ENABLED */
> /* #define HAL_NOR_MODULE_ENABLED */
> /* #define HAL_SRAM_MODULE_ENABLED */
> /* #define HAL_SDRAM_MODULE_ENABLED */
> /* #define HAL_HASH_MODULE_ENABLED */
> /* #define HAL_I2S_MODULE_ENABLED */
> /* #define HAL_IWDG_MODULE_ENABLED */
> /* #define HAL_LPTIM_MODULE_ENABLED */
> /* #define HAL_LTDC_MODULE_ENABLED */
> /* #define HAL_QSPI_MODULE_ENABLED */
> /* #define HAL_RNG_MODULE_ENABLED */
> /* #define HAL_RTC_MODULE_ENABLED */
> /* #define HAL_SAI_MODULE_ENABLED */
64,80c63,79
< /* #define HAL_MMC_MODULE_ENABLED */
< /* #define HAL_SPDIFRX_MODULE_ENABLED */
< /* #define HAL_SPI_MODULE_ENABLED */
< /* #define HAL_TIM_MODULE_ENABLED */
< /* #define HAL_UART_MODULE_ENABLED */
< /* #define HAL_USART_MODULE_ENABLED */
< /* #define HAL_IRDA_MODULE_ENABLED */
< /* #define HAL_SMARTCARD_MODULE_ENABLED */
< /* #define HAL_WWDG_MODULE_ENABLED */
< /* #define HAL_PCD_MODULE_ENABLED */
< /* #define HAL_HCD_MODULE_ENABLED */
< /* #define HAL_DFSDM_MODULE_ENABLED */
< /* #define HAL_DSI_MODULE_ENABLED */
< /* #define HAL_JPEG_MODULE_ENABLED */
< /* #define HAL_MDIOS_MODULE_ENABLED */
< /* #define HAL_SMBUS_MODULE_ENABLED */
< /* #define HAL_EXTI_MODULE_ENABLED */
---
> /* #define HAL_MMC_MODULE_ENABLED */
> /* #define HAL_SPDIFRX_MODULE_ENABLED */
> /* #define HAL_SPI_MODULE_ENABLED */
> /* #define HAL_TIM_MODULE_ENABLED */
> /* #define HAL_UART_MODULE_ENABLED */
> /* #define HAL_USART_MODULE_ENABLED */
> /* #define HAL_IRDA_MODULE_ENABLED */
> /* #define HAL_SMARTCARD_MODULE_ENABLED */
> /* #define HAL_WWDG_MODULE_ENABLED */
> /* #define HAL_PCD_MODULE_ENABLED */
> /* #define HAL_HCD_MODULE_ENABLED */
> /* #define HAL_DFSDM_MODULE_ENABLED */
> /* #define HAL_DSI_MODULE_ENABLED */
> /* #define HAL_JPEG_MODULE_ENABLED */
> /* #define HAL_MDIOS_MODULE_ENABLED */
> /* #define HAL_SMBUS_MODULE_ENABLED */
> /* #define HAL_EXTI_MODULE_ENABLED */
213c212
< #define ETH_RX_BUF_SIZE ETH_MAX_PACKET_SIZE /* buffer size for receive */
---
> #define ETH_RX_BUF_SIZE /* buffer size for receive */
diff -r --ex 661/Core/Src/main.c 670/Core/Src/main.c
218c218
< hsd1.Init.BusWide = SDMMC_BUS_WIDE_1B;
---
> hsd1.Init.BusWide = SDMMC_BUS_WIDE_4B;
diff -r --ex 661/Core/Src/syscalls.c 670/Core/Src/syscalls.c
13c13
< * Copyright (c) 2022 STMicroelectronics.
---
> * Copyright (c) 2020-2022 STMicroelectronics.
50c50
< 	return 1;
---
> return 1;
55,56c55,58
< 	errno = EINVAL;
< 	return -1;
---
> (void)pid;
> (void)sig;
> errno = EINVAL;
> return -1;
61,62c63,64
< 	_kill(status, -1);
< 	while (1) {}		/* Make sure we hang here */
---
> _kill(status, -1);
> while (1) {} /* Make sure we hang here */
67c69,70
< 	int DataIdx;
---
> (void)file;
> int DataIdx;
69,72c72,75
< 	for (DataIdx = 0; DataIdx < len; DataIdx++)
< 	{
< 		*ptr++ = __io_getchar();
< 	}
---
> for (DataIdx = 0; DataIdx < len; DataIdx++)
> {
> *ptr++ = __io_getchar();
> }
74c77
< return len;
---
> return len;
79c82,83
< 	int DataIdx;
---
> (void)file;
> int DataIdx;
81,85c85,89
< 	for (DataIdx = 0; DataIdx < len; DataIdx++)
< 	{
< 		__io_putchar(*ptr++);
< 	}
< 	return len;
---
> for (DataIdx = 0; DataIdx < len; DataIdx++)
> {
> __io_putchar(*ptr++);
> }
> return len;
90c94,95
< 	return -1;
---
> (void)file;
> return -1;
96,97c101,103
< 	st->st_mode = S_IFCHR;
< 	return 0;
---
> (void)file;
> st->st_mode = S_IFCHR;
> return 0;
102c108,109
< 	return 1;
---
> (void)file;
> return 1;
107c114,117
< 	return 0;
---
> (void)file;
> (void)ptr;
> (void)dir;
> return 0;
112,113c122,125
< 	/* Pretend like we always fail */
< 	return -1;
---
> (void)path;
> (void)flags;
> /* Pretend like we always fail */
> return -1;
118,119c130,132
< 	errno = ECHILD;
< 	return -1;
---
> (void)status;
> errno = ECHILD;
> return -1;
124,125c137,139
< 	errno = ENOENT;
< 	return -1;
---
> (void)name;
> errno = ENOENT;
> return -1;
130c144,145
< 	return -1;
---
> (void)buf;
> return -1;
135,136c150,152
< 	st->st_mode = S_IFCHR;
< 	return 0;
---
> (void)file;
> st->st_mode = S_IFCHR;
> return 0;
141,142c157,160
< 	errno = EMLINK;
< 	return -1;
---
> (void)old;
> (void)new;
> errno = EMLINK;
> return -1;
147,148c165,166
< 	errno = EAGAIN;
< 	return -1;
---
> errno = EAGAIN;
> return -1;
153,154c171,175
< 	errno = ENOMEM;
< 	return -1;
---
> (void)name;
> (void)argv;
> (void)env;
> errno = ENOMEM;
> return -1;

Based on this, I tried changing

hsd1.Init.BusWide = SDMMC_BUS_WIDE_4B;

to

hsd1.Init.BusWide = SDMMC_BUS_WIDE_1B;

in the 6.7.0 project and it fixed the issue. Note this is not the same as running the card in 1-bit mode, the FatFS Disk I/O driver switches it to 4-bit mode later in initialisation:

~/SDMMC_STM32CubeMX_Test/661 % rg "SDMMC_BUS_WIDE_4B"
Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_sd.c
2180: * @arg SDMMC_BUS_WIDE_4B: 4-bit data transfer
2202: else if(WideMode == SDMMC_BUS_WIDE_4B)
 
Drivers/STM32F7xx_HAL_Driver/Inc/stm32f7xx_ll_sdmmc.h
365:#define SDMMC_BUS_WIDE_4B SDMMC_CLKCR_WIDBUS_0
369: ((WIDE) == SDMMC_BUS_WIDE_4B) || \
 
Debug/661.list
10552: * @arg SDMMC_BUS_WIDE_4B: 4-bit data transfer
10597: else if(WideMode == SDMMC_BUS_WIDE_4B)
14765: if (HAL_SD_ConfigWideBusOperation(&hsd1, SDMMC_BUS_WIDE_4B) != HAL_OK)
 
FATFS/Target/bsp_driver_sd.c
62: if (HAL_SD_ConfigWideBusOperation(&hsd1, SDMMC_BUS_WIDE_4B) != HAL_OK)

I'm not quite sure what the whole sequence is for initialisation in the SD specification, but I think the card has to be in 1-bit mode first in order to set up 4-bit mode.

Amel NASRI
ST Technical Moderator
February 15, 2023

Hi @FPlow.1​ ,

An explanation of what was updated is provided by @Ghofrane GSOURI​ in this thread: SDCARD does not work (FR_NOT_READY) when migrating from FW_F4 V1.27.0 to newer FW_F4 V1.27.1.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.