Skip to main content
Nawres GHARBI
ST Technical Moderator
March 7, 2022
Question

STM32CubeMX 6.5.0 released

What is new in STM32CubeMX V6.5.0?

• Added the support for new part numbers in the STM32U5 Series: STM32U599NJHxQ, STM32U599BJYxQ, STM32U595ZJTxQ, STM32U5A9NJHxQ, STM32U5A9BJYxQ, STM32U5A5ZJTxQ and STM32U599NIHxQ.

• Added the support for new part numbers in the STM32C0 Series: STM32C011D6Yx, STM32C011F(4-6)Px, STM32C011F(4-6)Ux, STM32C011J(4-6)Mx, STM32C031C(4-6)Tx, STM32C031C(4-6)Ux, STM32C031K(4-6)Tx, STM32C031K(4-6)Ux, STM32C031G(4-6)Ux and STM32C031F(4-6)Px.

• Added the support for 2 new part numbers in the STM32F7 Series: STM32F723VCYxTR and STM32F723VEYxTR.

• Added the support for the P-L496G-CELL01 and P-L496G-CELL02 Discovery kits.

• Added enhancements of search criteria organized into categories, with more accurate commercial product information and with more specific documentation.

• Added the support for LPBAM firmware for the projects without Arm® TrustZone®(a) (TZEN=0) in the STM32U575/585 product line This new feature allows the easy design of low-power projects based on the powerful LPBAM firmware.

• Added the support for a default MPU configuration for the STM32H7 Series.

• Added the support for “Low Power Optimization configuration�?, including SMPS support, for the STM32U5 Series.

• Added the support of the EWARM compiler version v8.50. This version becomes the default proposed EWARM toolchain version for the STM32F7 Series, STM32F4 Series, STM32G0 Series, STM32G4 Series, STM32H7 Series, STM32U5 Series, and STM32C0 Series.

• Added the support for Azure® RTOS middleware bare-metal mode: – Azure® RTOS FileX for the STM32C0 Series and STM32U5 Series – Azure® RTOS LevelX for the STM32U5 Series

Known limitations

Please check the Release note

Main fixed issues

79064 [OPENAMP] Proxy feature.

79780 [UX] Source location path invalid in X-CUBE-MEMS1.

91324 [MX-ALL][Project Manager] Wrong firmware package when importing project. 109796 [MX-ALL][Makefile] Change the first assignment of variable CFLAGS from "=" to "+=".

117135 [MX-ALL][SAI] Give user the ability to always set the audio frequency.

118459 [MX-ALL][LTDC] Change the naming of the parameter “Not Data Enable Polarity�?. 119012 [STM32H7][MX-ADC][AWD1] “Analog watchdog Channel�? is automatically set to Channel 0 and cannot be modified.

119463 [STM32U575/585][MX-GPDMA] Wrong FIFO size for GPDMA1 channels from 0 to 3 in STM32CubeMX.

119999 [MX-MBEDTLS][STM32F4] The md5.c file is not copied into the project directory after defining the MBEDTLS_MD5_C module.

120035 [LL][MX-UART][MX-Code generation] Wrong attribute in LL_USART_SetRXPinLevel().

Link

https://www.st.com/en/development-tools/stm32cubemx.html#overview

This topic has been closed for replies.

1 reply

sirius506
Associate III
March 8, 2022

I'm glad to find that new CubeMX also brings new CubeFW releases.

I noticed that new CubeF4 and CubeH7 releases comes with updated USB Device library (v2.10.0) which supports new class drivers and composite device. However, I can't find the MX GUI to supports these features. How can I configure these new features?