Skip to main content
TCL.1
Visitor II
May 28, 2021 5:14 AM UTC
Question

STM32CubeMX 6.2.0 generate MDK-ARM V5.27 project without R/O,R/W base causing image mapping error

STM32CubeMX project for STM32F407ZG

Firmware pack FW_F4 V1.26.1

generated project : Option for Target -> Linker -> R/O Base, R/W Base is not configurated which cause Image Entry point wrongly set to 0x00008001

This topic has been closed for replies.

1 reply

Khouloud ZEMMELI
ST Employee
Jun 4, 2021 9:30 AM UTC

Hello @TCL.1​ ,

Thank you for your post,

Actually, the default setting is taken from "Memory layout of Target Dialog" as it's checked by default, in case you want to change R/O Base and R/W Base, you need to uncheck this parameter.

Could you please give me more details about the problem that you have encountered ?

Thanks, Khouloud