Skip to main content
Associate III
Nov 21, 2026 9:39 PM UTC
Question

STM32CubeMX 6.19.0 – Save As fails for all projects, including previously working ones

Hello ST team,

I encountered an issue with the Save As function in STM32CubeMX V6.19.0.

I am working with a B-WB1M-WPAN1 (STM32WB1MMC) project using STM32Cube_FW_WB V1.25.0 and IAR EWARM 9.70.

During project migration, I opened an .ioc configuration file named BLE_Data_WB1M_FAST_01.ioc, which had been modified manually outside STM32CubeMX.

After working with this configuration, I discovered that File → Save As no longer works correctly. In one attempt, the operation resulted in an "Access is denied" error.

The most important observation is that Save As also fails with older, unrelated projects that were not modified.

At the same time:

  • Existing projects can still be opened.

  • Normal Save works.

  • Generate Code works.

  • IAR EWARM project files are generated successfully.

Workaround:

I managed to continue working by manually copying the project directory to a new location, renaming the project to match the new directory name, and then using the normal Save and Generate Code commands.

However, the Save As functionality itself remains unavailable.

My questions:

  1. Is this a known STM32CubeMX issue?

  2. Can opening or processing an externally modified .ioc file affect the Save As functionality for other projects?

  3. Does CubeMX maintain any global configuration, cache, or project history that could cause this behavior?

  4. How can I restore Save As without reinstalling STM32CubeMX or losing existing configuration settings?

  5. Are there diagnostic logs I can provide to help identify the problem?

I cannot confirm that the manually modified .ioc file caused the issue, but the problem was discovered after working with it.

Thank you for your assistance.