Skip to main content
ruddy17
Associate
March 24, 2026
Solved

STM32CubeMX 6.17 FreeRTOS CMSIS-V2: some params missing from IOC/model, generated as (valueNotSetted)

Hello,

I found a CubeMX database issue affecting STM32H747 dual-core projects using FreeRTOS with CMSIS-RTOS V2.

Environment

MCU: STM32H747
Cube/HAL: STM32CubeH7 1.13.x
CubeMX: 6.17
FreeRTOS: 10.6.2

Problem

Two FreeRTOS configuration parameters are not present in the MicroXplorer Configuration settings and are not retained in the internal IOC model:

configUSE_SB_COMPLETED_CALLBACK
configUSE_MINI_LIST_ITEM

Because of that, code generation can produce invalid output in FreeRTOSConfig.h such as:

#define configUSE_MINI_LIST_ITEM ( valueNotSetted )
#define configUSE_SB_COMPLETED_CALLBACK ( valueNotSetted )

This breaks the build and/or downstream FreeRTOS code.

Editing the .ioc manually does not solve it permanently, because CubeMX overwrites the .ioc on regeneration.

Adding manual defines in USER CODE blocks is only a local workaround and does not fix the root cause.

Root cause found

The issue appears to be in the CubeMX FreeRTOS mode database, not in the generated project itself.

For STM32H747, CubeMX uses a FreeRTOS mode definition named FREERTOS-v8.0.0_Cube_Modes.xml for the UI/model layer, even though the generated FreeRTOS content/template is 10.6.2.

Inside that mode file, the two missing parameters were defined with a condition using: S_CMSIS_RTOS_V2


But for H747 dual-core per-context FreeRTOS instances, they need to be context-aware like the neighboring parameters, for example: S_CMSIS_RTOS_V2$context.
 

Without $context, those parameters are not properly exposed or persisted for the per-core FreeRTOS instances.

Local fix that works

In the CubeMX database file db/mcu/IP/FREERTOS-v8.0.0_Cube_Modes.xml, change the condition for configUSE_SB_COMPLETED_CALLBACK from S_CMSIS_RTOS_V2 to S_CMSIS_RTOS_V2$context.

Do the same for configUSE_MINI_LIST_ITEM, again changing S_CMSIS_RTOS_V2 to S_CMSIS_RTOS_V2$context.

After this change, the issue is fixed on my side.

Additional defensive fix

To prevent broken generation even if the parameters are still missing in some cases, I also added fallback defaults in the FreeRTOS H7 template file db/templates/freertos_conf_v10_6_2_cmsis_v2.ftl.

The defaults I added were:

  • valueUSE_SB_COMPLETED_CALLBACK = 0
  • valueUSE_MINI_LIST_ITEM = 1

This avoids generation of valueNotSetted in FreeRTOSConfig.h.

Why this is confusing

CubeMX shows or generates FreeRTOS 10.6.2, but the bug is in the v8.0.0_Cube mode XML.

From debugging this, it looks like:

  • the v8.0.0_Cube file is the CubeMX metadata and UI layer
  • the 10.6.2 files are the actual generation and template layer

So the wrong behavior comes from the UI/model database, while the generated template already expects the two parameters correctly.

Expected behavior

For STM32H747 FreeRTOS CMSIS-V2 projects, CubeMX should:

  • expose configUSE_SB_COMPLETED_CALLBACK
  • expose configUSE_MINI_LIST_ITEM
  • persist them in the internal model and IOC
  • generate valid values in FreeRTOSConfig.h

Observed behavior

CubeMX omits those settings from the model/UI for H747 and can generate invalid FreeRTOSConfig.h output where configUSE_MINI_LIST_ITEM and configUSE_SB_COMPLETED_CALLBACK are set to valueNotSetted.

Request

Please fix the FreeRTOS mode database for H747 dual-core/per-context handling so these two parameters use the correct context-aware condition and are always generated with valid values.

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
March 25, 2026

Hello @ruddy17 

Your detailed explanation is much appreciated.

Issue has been escalated to dev team under internal ticket ID #0060998

I will keep you posted with updates.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Explorer
March 24, 2026

I can confirm this is a real CubeMX code generation bug.

With newer FreeRTOS, CubeMX generated the following invalid setting in FreeRTOSConfig.h:
#define configUSE_MINI_LIST_ITEM ( valueNotSetted )


Because this is used in preprocessor #if expressions, it effectively behaves as 0. In newer FreeRTOS versions this changes the internal layout of List_t / MiniListItem_t.

As a result, FreeRTOS thread-aware debugging breaks. In my case:

  • J-Link + Cortex-Debug + FreeRTOS awareness stopped working correctly
    breakpoints were unreliable
    stepping often crashed GDB
    debugger logs showed failures reading FreeRTOS task stack frames
Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
March 25, 2026

Hello @ruddy17 

Your detailed explanation is much appreciated.

Issue has been escalated to dev team under internal ticket ID #0060998

I will keep you posted with updates.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.