Skip to main content
DClif.1
Associate
Jan 7, 2026 2:23 PM UTC
Question

STM32CubeMX 6.16.1 linux installer issuers (Bazzite/Fedora 43)

I'm running Bazzite (Fedora 43) and tried to install STM32CubeMX on a Fedora distrobox and was met with some issues.

First, the installer is unable use /bin/chmod, this is fixed by switching out the installer's `jre\bin` directory for OpenJDK.

Second, if you run as a normal user it fails with:

com.izforge.izpack.api.exception.IzPackException: An error occured in java.lang.Thread.run() at Thread.java:1583 in com.izforge.izpack.installer.unpacker.UnpackerBase.run() at UnpackerBase.java:241 in com.izforge.izpack.installer.unpacker.UnpackerBase.unpack() at UnpackerBase.java:319 Caused by: com.izforge.izpack.api.exception.InstallerException: File execution failed in com.izforge.izpack.installer.unpacker.UnpackerBase.unpack() at UnpackerBase.java:299 in com.izforge.izpack.installer.unpacker.UnpackerBase.unpack() at UnpackerBase.java:483 in com.izforge.izpack.installer.unpacker.UnpackerBase.executeFiles() at UnpackerBase.java:959


This is fixed by running the installer via sudo.

This is what I did to get it running in distrobox:

  • Installing STM32CubeMX on linux
    • Unpack the .zip file.
    • Install it:
    • 	 cd 
      	 distrobox create --name stm32cubemx
      	 distrobox enter stm32cubemx
      	 sudo dnf install java-latest-openjdk.x86_64
      	 mv jre jre.st
      	 mkdir jre
      	 ln -s /usr/bin jre/bin
      	 chmod +x SetupSTM32CubeMX-6.16.1
      	 sudo ./SetupSTM32CubeMX-6.16.1
    • Create a desktop file (in the container)
      • 		 cd /usr/local/STMicroelectronics/STM32Cube/STM32CubeMX/
        		 sudo nano STM32CubeMX.desktop
      • Add the content as follows:
      • 		 [Desktop Entry]
        		 Version=6.16.1
        		 Name=STM32CubeMX-6.16.1
        		 Comment=STM32CubeMX Application for STM32 development
        		 Exec=/usr/local/STMicroelectronics/STM32Cube/STM32CubeMX/STM32CubeMX
        		 Icon=stm32cubemx
        		 Terminal=false
        		 Type=Application
        		 Categories=Development;
    • Export the desktop file (in the container)
      • 		 distrobox-export --app /usr/local/STMicroelectronics/STM32Cube/STM32CubeMX/STM32CubeMX.desktop
    • Then run the app from the host's app launcher, e.g. KRunner. It will appear as STM32CubeMX (on stm32cubemx)


With this, I'm able to run 6.16.1, but the MCU selector, board selected and various other progress dialog windows are just empty with a white background.  It does load up existing projects however.

Other users report that 6.16 has rendering issues on Fedora 43.

I was able to install CubeMX 6.15 from the Baazar store (flatpak) just fine, and that doesn't have any issues rendering the MCU selector or other dialog windows.

5 replies

ST Technical Moderator
Jan 7, 2026 2:44 PM UTC

Hello @DClif.1 

Based on RN0094 : 1.2 Host PC system requirements, Fedora 43 is not yet supported with STM32CubeMX.

Below are the supported operating systems and architectures for CubeMX 6.16.1:

• Windows® 10 and 11, 64 bits (x64)(b)
• Linux®: Ubuntu® LTS 22.04 and LTS 24.04, and Fedora® 42(c) (d) (e)
• macOS® 15 (Sequoia), macOS® 26 (Tahoe)(f)

KR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
DClif.1
DClif.1Author
Associate
Jan 8, 2026 11:45 AM UTC

Yes, I became aware of the Fedora 43 limitation.

However, related to this, I tried using 6.15.0 via distrobox and had no installer errors, but still had the same missing window content issues as 6.16.1 did.  that is: every pop-up window was empty - window frame, but with no content and just a white background.

flathub has a version of CubeMX, but it is out of date, the version there is 6.15.0 - https://flathub.org/en/apps/com.st.STM32CubeMX

Can you could pass on my experience to the developers so that these issues can be fixed in a future version, or do I need to open a ticket somewhere?

Visitor II
Jan 11, 2026 4:57 AM UTC

I just installed version 6.16.1 of STM32CubeMX without any issues.  I just downloaded stm32cubemx-lin-v6-16-1.zip and entered the following commands to install it:

$ unzip stm32cubemx-lin-v6-16-1.zip
$ sudo ./SetupSTM32CubeMX-6.16.1

Run STM32CubeMX with the following command:

$ /usr/local/STMicroelectronics/STM32Cube/STM32CubeMX/STM32CubeMX

 Root permissions were needed for installation, but not execution.

Visitor II
Apr 21, 2026 7:01 PM UTC

I have just tested this with CubeMX 6.17 and Ubuntu 24.04 in a Distrobox container and it is still broken with blank popup windows. I checked out the Flatpak version and that works great. Looking into how they do it I don't see anything special apart from them installing OpenJDK and not using the bundled JRE.