Skip to main content
Semer CHERNI
ST Employee
Nov 27, 2024 9:17 AM UTC
Question

STM32CubeMX 6.13.0 released

We are pleased to announce to you that the release 6.13.0 of STM32CubeMX is available.

What is new in 6.13.0:

  • Added support for the following series, microcontrollers and microprocessors: STM32N6, STM32U3, STM32WL3x, STM32G411xx and STM32C0
  • Added the support for the following Nucleo boards: NUCLEO-N657X0-Q, NUCLEO-C051C8, NUCLEO-C092RC, NUCLEO-U385RG-Q, NUCLEO-WL33CC1 and NUCLEO-WL33CC2
  • Added the support for a new Discovery kits and a new expansion boards: STM32N6570-DK and B-WBA5M-WPAN
  • Extended the implementation of the CMake and Makefile build generators taking into account the memory management tool (MMT) features:
    • Single-core microcontrollers without Arm® TrustZone®(a), excluding STM32H7Rx/7Sx, or with disabled TrustZone®
    • Dual-core microcontrollers without TrustZone® (such as in the STM32H7 series)
  • Add the support of the memory management tool on STM32H7 dual-core and STM32WBA5Mxx microcontrollers
  • Added the compare projects feature to make user able to differentiate between two STM32CubeMX project files across different microcontrollers and microprocessors.
  • Implemented the loading of the firmware or applications code from the external memory (EXTMEMLOADER) using the OpenBootloader interface for STM32H7Rx/7Sx.

Main fixed issues in 6.13.0:

Refer to the STM32 microcontroller wiki at:
https://wiki.st.com/stm32mcu/wiki/Category:STM32CubeMX_errata

Known problems and limitations:

Refer to the STM32 microcontroller wiki at:

https://wiki.st.com/stm32mcu/wiki/STM32CubeMX_errata_6.13.x

How to get STM32CubeMX 6.13.0:

  • Under this link
  • Or update your current installation of STM32CubeMX using: Help > Check for updates
This topic has been closed for replies.

5 replies

Andrew Neil
Super User
Nov 27, 2024 9:31 AM UTC

@Semer CHERNI wrote:

Main fixed issues in 6.13.0:

Refer to the STM32 microcontroller wiki at:
https://wiki.st.com/stm32mcu/wiki/Category:STM32CubeMX_errata


There is no Errata for v6.13.0:

AndrewNeil_0-1732699860263.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
TLI.11
ST Employee
Dec 3, 2024 8:11 AM UTC
MQi.1
Senior II
Dec 9, 2024 3:14 AM UTC

When downloaded the latest version here - https://www.st.com/en/development-tools/stm32cubemx.html, ant unzip it on Ubuntu, got these:

 

 

unzip en.*.zip
Archive: en.stm32cubemx-lin-v6-12-0.zip
 End-of-central-directory signature not found. Either this file is not
 a zipfile, or it constitutes one disk of a multi-part archive. In the
 latter case the central directory and zipfile comment will be found on
 the last disk(s) of this archive.
unzip: cannot find zipfile directory in one of en.stm32cubemx-lin-v6-12-0.zip or
 en.stm32cubemx-lin-v6-12-0.zip.zip, and cannot find en.stm32cubemx-lin-v6-12-0.zip.ZIP, period.

 

 

how to fix it?

Associate
Dec 30, 2024 8:09 PM UTC

Hello Semer Cherni,

STM32CubeMX 6.13.0 "Known problems and limitations" fails to point out that dual-core mcus are still not fully supported (development and debugging)

Please see: https://community.st.com/t5/stm32cubemx-mcus/stm32h7-dual-core-support/td-p/215764

Not having all the boot modes defeats the purpose of having CubeMX because the changes have to be manually remade in the IDE everytime a small change is made in CubeMX.

 

 

MKanc.1
Associate III
Jan 27, 2025 2:27 AM UTC

NUCLEO-U385RG-Q ??