Skip to main content
xlrl
Associate III
April 19, 2025
Solved

STM32CubeMX 6.13.0 not generating calls to HAL_DMA_IRQHandler in GPDMA1_Channel0_IRQHandler

In our project we are using GPDMA for SAI transfers:

  • STM32CubeMX 6.13.0

  • STM32Cube_FW_U5_V1.7.0

  • STM32U535RE target

  • X-CUBE-FREERTOS 1.3.0 (FreeRTOS 10.6.2)

Description of the behaviour:

  • We this .ioc configuration STM32CubeMX does not create the calls to `HAL_DMA_IRQHandler`.
  • Note: in the past the time base call also was not generated (TIM6)
  • A different .ioc we were using for the NUCLEO board was producing the correct/expected code

Example of expected code:

void GPDMA1_Channel0_IRQHandler(void)
{
 /* USER CODE BEGIN GPDMA1_Channel0_IRQn 0 */

 /* USER CODE END GPDMA1_Channel0_IRQn 0 */
 HAL_DMA_IRQHandler(&handle_GPDMA1_Channel0);
 /* USER CODE BEGIN GPDMA1_Channel0_IRQn 1 */

 /* USER CODE END GPDMA1_Channel0_IRQn 1 */
}

Actually generated code (note the missing call):

void GPDMA1_Channel0_IRQHandler(void)
{
 /* USER CODE BEGIN GPDMA1_Channel0_IRQn 0 */

 /* USER CODE END GPDMA1_Channel0_IRQn 0 */
 /* USER CODE BEGIN GPDMA1_Channel0_IRQn 1 */

 /* USER CODE END GPDMA1_Channel0_IRQn 1 */
}

 Workaround:

void GPDMA1_Channel0_IRQHandler(void)
{
 /* USER CODE BEGIN GPDMA1_Channel0_IRQn 0 */
 HAL_DMA_IRQHandler(&handle_GPDMA1_Channel0);
 // comment out generated code, so a future generation
 // run does not create duplicate calls
#if 0
 /* USER CODE END GPDMA1_Channel0_IRQn 0 */
 /* USER CODE BEGIN GPDMA1_Channel0_IRQn 1 */
#endif
 /* USER CODE END GPDMA1_Channel0_IRQn 1 */
}
This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
April 21, 2025

Hello @xlrl 

Using your .ioc file, I've been able to generate the code expected:

void GPDMA1_Channel0_IRQHandler(void)
{
 /* USER CODE BEGIN GPDMA1_Channel0_IRQn 0 */

 /* USER CODE END GPDMA1_Channel0_IRQn 0 */
 HAL_DMA_IRQHandler(&handle_GPDMA1_Channel0);
 /* USER CODE BEGIN GPDMA1_Channel0_IRQn 1 */

 /* USER CODE END GPDMA1_Channel0_IRQn 1 */
}

I've just made a change on the .ioc file setting the "Call HAL handler" option for this interrupt:

STTwo32_0-1745218899359.png

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

6 replies

STTwo-32
ST Technical Moderator
April 19, 2025

Hello @xlrl 

Do you have the same issue will using the STM32CubeMX V6.14.1?

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
xlrl
xlrlAuthor
Associate III
April 20, 2025

Yes, only a few comments changed.

STTwo-32
ST Technical Moderator
April 20, 2025

Hello @xlrl 

Thank you so much for escalating this. I will have a look at this. Please add your .ioc file (based on the V6.14.1 of the STM32CubeMX).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.