Skip to main content
SOfne.1
Associate II
November 27, 2024
Question

STM32CubeMX 6.11.0 and STM32CubeIDE 1.15.1: bug when using DMA2 with low-level drivers

Used STM32CubeIDE version: 1.15.1
Used driver library: STM32Cube_FW_G0_V1.6.2, LowLevel-Drivers
Microcontroller STM32G0B0xx

 

LL Drivers have been selected for DMA and all other peripherals as far as possible.

 

There are several bugs in the generated code.

Bug #1

Even though LL drivers should be used, MX_DMA_Init() looks like this:

 

/**
 * Enable DMA controller clock
 */
void MX_DMA_Init(void)
{

 /* Init with LL driver */
 /* DMA controller clock enable */
 LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);
 __HAL_RCC_DMA2_CLK_ENABLE(); // <- Should be LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA2) instead!

 /* DMA interrupt init */
 /* DMA1_Channel1_IRQn interrupt configuration */
 NVIC_SetPriority(DMA1_Channel1_IRQn, 1);
 NVIC_EnableIRQ(DMA1_Channel1_IRQn);
 /* DMA1_Channel2_3_IRQn interrupt configuration */
 NVIC_SetPriority(DMA1_Channel2_3_IRQn, 1);
 NVIC_EnableIRQ(DMA1_Channel2_3_IRQn);
 /* DMA1_Ch4_7_DMA2_Ch1_5_DMAMUX1_OVR_IRQn interrupt configuration */
 NVIC_SetPriority(DMA1_Ch4_7_DMA2_Ch1_5_DMAMUX1_OVR_IRQn, 1);
 NVIC_EnableIRQ(DMA1_Ch4_7_DMA2_Ch1_5_DMAMUX1_OVR_IRQn);

}

 

Bug #2

I use DMA for USART. The DMA initialization code generated in MX_USART6_UART_Init() is invalid:

 

void MX_USART6_UART_Init(void)
{
 // ...
 /* USART6 DMA Init */

 /* USART6_RX Init */
 LL_DMA_SetPeriphRequest(DMA2_Channel3, DMA2_Channel3, LL_DMAMUX_REQ_USART6_RX); // Should look like this: LL_DMA_SetPeriphRequest(DMA2, LL_DMA_CHANNEL_3, LL_DMAMUX_REQ_USART6_RX), following lines are invalid, too

 LL_DMA_SetDataTransferDirection(DMA2_Channel3, DMA2_Channel3, LL_DMA_DIRECTION_PERIPH_TO_MEMORY);

 LL_DMA_SetChannelPriorityLevel(DMA2_Channel3, DMA2_Channel3, LL_DMA_PRIORITY_HIGH);

 LL_DMA_SetMode(DMA2_Channel3, DMA2_Channel3, LL_DMA_MODE_NORMAL);

 LL_DMA_SetPeriphIncMode(DMA2_Channel3, DMA2_Channel3, LL_DMA_PERIPH_NOINCREMENT);

 LL_DMA_SetMemoryIncMode(DMA2_Channel3, DMA2_Channel3, LL_DMA_MEMORY_INCREMENT);

 LL_DMA_SetPeriphSize(DMA2_Channel3, DMA2_Channel3, LL_DMA_PDATAALIGN_BYTE);

 LL_DMA_SetMemorySize(DMA2_Channel3, DMA2_Channel3, LL_DMA_MDATAALIGN_BYTE);

 /* USART6_TX Init */
 LL_DMA_SetPeriphRequest(DMA2_Channel4, DMA2_Channel4, LL_DMAMUX_REQ_USART6_TX);

 LL_DMA_SetDataTransferDirection(DMA2_Channel4, DMA2_Channel4, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);

 LL_DMA_SetChannelPriorityLevel(DMA2_Channel4, DMA2_Channel4, LL_DMA_PRIORITY_HIGH);

 LL_DMA_SetMode(DMA2_Channel4, DMA2_Channel4, LL_DMA_MODE_NORMAL);

 LL_DMA_SetPeriphIncMode(DMA2_Channel4, DMA2_Channel4, LL_DMA_PERIPH_NOINCREMENT);

 LL_DMA_SetMemoryIncMode(DMA2_Channel4, DMA2_Channel4, LL_DMA_MEMORY_INCREMENT);

 LL_DMA_SetPeriphSize(DMA2_Channel4, DMA2_Channel4, LL_DMA_PDATAALIGN_BYTE);

 LL_DMA_SetMemorySize(DMA2_Channel4, DMA2_Channel4, LL_DMA_MDATAALIGN_BYTE);

 /* USART6 interrupt Init */
 // ...
}

 

 

As far as I can see in the release notes of the newer STM32CubeMX this problem has not been fixed yet.

This topic has been closed for replies.

1 reply

ST Technical Moderator
November 27, 2024

Hello @SOfne.1 

There is a new STM32CubeMx release v6.13 with enhancement and fixes.

Please try this latest release and keep me informed about your updates.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks