Skip to main content
VPrib
Visitor II
Jun 14, 2019 6:20 AM UTC
Question

STM32CubeMX-5.2.1 installation path

STM32CubeMX-5.2.1 - why I can't install it in d:\STM32\STM32CubeMX path?

I use d:\STM\ for \STM32 ST-LINK Utility\ , \STMStudio\ and other STM application. Why not CubeMX?

Setup returns error: Invalid directory path. Please enter a directory path meets the operation system's requirements.

This topic has been closed for replies.

4 replies

Miguel XRay
Associate
Jul 30, 2019 9:23 AM UTC

Same problem to me, on Windows 10 (64 bit), no install directory will make it happy, I cannot install the software.

GokhanBektas
Visitor II
Aug 8, 2019 11:06 PM UTC

You need to use capitalized drive letter "D" instead of "d"

Then it should work fine.

Miguel XRay
Associate
Aug 27, 2019 8:10 AM UTC

Thanks a lot, it works.

This is a really stupid bug, but your answer is of great use!

NBlas.1
Associate
Aug 23, 2020 6:56 PM UTC

GokhanBektas thanks for the contribution please but sometimes capitalizing the drive letter doesn't work . When I faced the same problem, I only when into that directory/path and permanently deleted the folder STM32Cube, then when I continued with the installation, it went on successfully.