Skip to main content
Kent Swan
Associate III
Apr 22, 2019 4:34 AM UTC
Question

STM32CubeMX 5.1.0 eclipse plugin to System regen failure

Using System Workbench 5.8 and 5.9 (both have same issue) with eclipse CubeMX plug in 5.1.0. Target device STM32L462RE. Library is STM32Cube FW_L4 V1.13.0. Initial project and code generation is fine. Launching STLINK-V2 works normally. When making subsequent cubeMX changes STM32L462RETx_FLASH.ld goes from normal to an empty file and debug launch is no longer possible. Restoring the .ld file from a backup area allows debug launch again. BAD Dog.

This topic has been closed for replies.

1 reply

S.Ma
Principal
Apr 22, 2019 6:13 AM UTC

Are we going to have another post tomorrow with similar topic and different title to remain on top of the post list? ;)

When starting a project, like in automotive, freeze your tools and toolschain to a fixed version so you can find bug origins only to HW and FW.

Or update toolschain without changing FW and HW when absolutely necessary.