Skip to main content
butenko
Visitor II
April 29, 2015
Question

STM32CubeMX 4.7.1 Bug Report: Keil info for STLINK/Trace

  • April 29, 2015
  • 1 reply
  • 735 views
Posted on April 30, 2015 at 01:40

After upgrading to Subj, the Keil uVision STLink Debugger Trace options are reset each time STM32CubeMX generates code.

To reproduce;

using Keil uVision 5.14.0.0 (the current version), open ''Options for Target XXX'' -> Debug -> STLink Debugger/Settings -> Trace.

Select ''Trace Enable'' and modify some other settings (such as the Core Clock and ITM Stimulus Port, for example).

Save, restart Keil uVision to make sure the new options stay in place.

Use   STM32CubeMX  to generate code again, open the project uVision, bring up Debug Trace options, see the specified options gone (reset to default).

It looks like the newly release 4.7.1 version of Cube removes the following section from the  <TargetDriverDllRegistry/> element from the project.uvoptx  XML file.

The problem did not exist in STM32CubeMX 4.7.0.

#stm32cubemx #stlink #cube
This topic has been closed for replies.

1 reply

stm32cube-t
ST Employee
June 4, 2015
Posted on June 04, 2015 at 18:39

Hello, this is fixed with MX 4.8.

Best regards