Skip to main content
Associate II
June 20, 2025
Solved

STM32cubeIDE generates incorrect linker script for STM32U073C8T6

When starting a new project in the STM32cubeIDE and selecting the STM32U073C8T6 as the microcontroller, which has 64k flash and 40k RAM, the generated linker script uses 256k flash and 32k RAM.

 

Jochem_0-1750416445868.png

Also the description says that this device has 256k flash.

Jochem_1-1750416524327.png

Is this a bug and if so how can this be fixed?

How can the linker script be updated to use the correct flash and RAM size?

This topic has been closed for replies.
KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
June 20, 2025

Hello @Jochem and welcome to the community;

 

Could you please precise which STM32CubeIDE and STM32CubeMX versions are you using?

I'm unable to reproduce the issue with STM32CubeIDE 1.18.0 version and with STM32CubeMX 6.14.1 version to generate the code.

KDJEM1_0-1750418167105.png

I recommend you to download the latest versions of STM32CubeIDE and STM32CubeMx toolchains.  

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

3 replies

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
June 20, 2025

Hello @Jochem and welcome to the community;

 

Could you please precise which STM32CubeIDE and STM32CubeMX versions are you using?

I'm unable to reproduce the issue with STM32CubeIDE 1.18.0 version and with STM32CubeMX 6.14.1 version to generate the code.

KDJEM1_0-1750418167105.png

I recommend you to download the latest versions of STM32CubeIDE and STM32CubeMx toolchains.  

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
JochemAuthor
Associate II
June 20, 2025

I was on version 1.17.0 of the STM32cubeIDE, I'm now upgrading and will check again then.

I noticed when I make a project with this setting

Jochem_0-1750418887031.png

In version 1.17.0 the linker script is correct.

After updating to version 1.18.1 the linker script is also correct when selecting STM32Cube.

Thanks for the help.

Andrew Neil
Super User
June 20, 2025

@Jochem wrote:

How can the linker script be updated to use the correct flash and RAM size?


It's just a plain text file;  you can edit it in any text editor - including the IDE's text editor.

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.