Skip to main content
Jvan .31
Associate
Feb 20, 2020 12:11 AM UTC
Question

STM32CubeIDE fails to generate main.c correctly form IOC file

Hi all, been working on my project for a while with great success using a STM32L496.

As of late when I generate code from my .ioc file that it fails to to add the function name for the GPIO initialization function. Herewith the code generated:

/**

 * @brief GPIO Initialization Function

 * @param None

 * @retval None

 */

{

 GPIO_InitTypeDef GPIO_InitStruct = {0};

Note the lack of a function name.

I've deleted main.c and re-created. Same result. Note that the GPIO Initi function is also missing from main. Apart from this everything else seems to be ok.

Any suggestions?

This topic has been closed for replies.

2 replies

Markus GIRDLAND
ST Employee
Feb 20, 2020 12:17 PM UTC

Do you know a way to recreate this for another project? Or could you share the .ioc file and I'll see if I get the same thing?

Jvan .31
Jvan .31Author
Associate
Feb 23, 2020 9:55 PM UTC

Please find attached the IOC file