Skip to main content
AErde.1
Associate
Jun 15, 2020 1:41 PM UTC
Question

STM32CubeIDE doesn't generate UART init function call

I am using NUCLEO-H743ZI which has STM32H743ZI on it. In the 'Device Configuration Tool' under the 'Project Manager'->'Advance Settings' there are options to set how I want to generate HAL calls. I basically want to set all of them 'Visibility(Static)' so they are called at the 'beginning' of main function.

However as soon as I hit 'Save' or 'Generate Code' the visibility of 'MX_USART3_UART_Init' disabled and 'Not Generate Function Call' is selected automatically. I can of course call the function manually but this unpredictable behaviour is concerning...

0693W000001qixjQAA.png

This topic has been closed for replies.

6 replies

Peter BENSCH
ST Technical Moderator
Jun 16, 2020 1:50 PM UTC

Are you able to attach the IOC file to check the behavior?

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Khouloud ZEMMELI
ST Employee
Jun 18, 2020 12:04 PM UTC

​Hi @AErde.1​ 

Please use the latest CubeMX version (5.6.1), if issue still exist , could you please share your ioc file?

Thanks

Khouloud

AErde.1
AErde.1Author
Associate
Jun 18, 2020 1:04 PM UTC

Thank you for your responses, my CubeMX version is 5.6.1 and CubeIDE version is 1.3.1

I would like to give update about my situation. Even though tool doesn't allow me to set static visibility, it has been called somewhere inside CubeAI with CubeAI's generated code. Hence it seems working, but as soon as I disable "CubeAI Validation" the settings are left as it is so UART is left uninitialized.

This kind of dynamic between the plugins and CubeMX is little hard to discover especially since this function visibility is under 'Advanced Settings' which can be tricky for inexperinced users such as me.

Khouloud ZEMMELI
ST Employee
Jun 24, 2020 10:21 AM UTC

​Thanks @AErde.1​  for your feedback , issue detected, it will be fixed.

Best regards,

Khouloud

Visitor II
Mar 18, 2025 12:00 PM UTC

Is the problem solved? I am having the same problem with the same board

Visitor II
Apr 24, 2025 6:20 AM UTC

I guess its not. I am using h755zi and this cannot generate the code at all