Skip to main content
AVoel.1
Associate III
Jul 9, 2020 9:34 PM UTC
Question

STM32CubeIDE and STM32CubeMx bugs on Mac Catalina

These two bugs seem related.

Bug 1 on STM32CubeIDE. After modifying an ioc file, when you regenerate, the IDE wipes all the contents of the Drivers folder and all subfolders, and doesn't replace them! Yow.

Bug2 on STM32CubeMx. When generating code, the Core files are successfully created, but then STM32CubeMx hangs indefintely trying to create libraries.

Probably some problem with write permissions on Mac Catalina...

This topic has been closed for replies.

2 replies

Khouloud ZEMMELI
ST Employee
Dec 2, 2020 9:47 AM UTC

Hi @AVoel.1​ ,

Are you still facing same issues with the latest CubeMX version (6.1.0) ?

Khouloud

AVoel.1
AVoel.1Author
Associate III
Dec 2, 2020 4:11 PM UTC

No, actually. The problem went away by itself. I'm not sure if it was because of an update or not, but in any case, all is well. I'm grateful that ST is supporting the Mac OS platform. I abandoned Windows during the Windows 8 debacle and every time I have to do something in Windows I have to hold my nose. I was actually happy with Windows 7, I don't know why MS took such a wrong turn.