Skip to main content
Associate III
January 13, 2026
Solved

STM32CubeIDE 2.0.0 problems with generated STM32WB5MMG code

Hi @TDK ,

I have just downloaded and installed the new version 2.0.0 of the IDE and the MX software (since it is no longer integrated). I was working on a project based on the STM32WB5MMG, and everything was working correctly with IDE version 1.19.0 and STM32Cube FW_WB V1.23.0.

After opening the project and regenerating the code with the new IDE version and STM32Cube FW_WB V1.24.0, I noticed some issues:

  1.  in custom_stm.c it generates two times this variables:
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
uint16_t SizeFw_Ver = 1;
uint16_t SizeDatetime = 7;
uint16_t SizeStatus = 6;
uint16_t SizeMonitor = 15;
uint16_t SizeEnv_Data = 90;
uint16_t SizeFw_Ver = 1;
uint16_t SizeDatetime = 7;
uint16_t SizeStatus = 6;
uint16_t SizeMonitor = 15;
uint16_t SizeEnv_Data = 90;​

2. it doesn't generate any local functions in custom_app.c:

/* USER CODE END FD */

/*************************************************************
 *
 * LOCAL FUNCTIONS
 *
 *************************************************************/

/* INFORMATION */
/* ENVIRONMENTAL */

/* INFORMATION */
/* ENVIRONMENTAL */

/* USER CODE BEGIN FD_LOCAL_FUNCTIONS*/
/* USER CODE END FD_LOCAL_FUNCTIONS*/

when before there were some function for characteristic notification (I leave here an example):

/*************************************************************
 *
 * LOCAL FUNCTIONS
 *
 *************************************************************/

/* INFORMATION */
/* ENVIRONMENTAL */
__USED void Custom_Env_data_Update_Char(void) /* Property Read */
{
 uint8_t updateflag = 0;

 /* USER CODE BEGIN Env_data_UC_1*/

 /* USER CODE END Env_data_UC_1*/

 if (updateflag != 0)
 {
 Custom_STM_App_Update_Char(CUSTOM_STM_ENV_DATA, (uint8_t *)UpdateCharData);
 }

 /* USER CODE BEGIN Env_data_UC_Last*/

 /* USER CODE END Env_data_UC_Last*/
 return;
}

How I can fix the problem?

Thanks.

ST Technical Moderator
January 19, 2026

Hello @matteverze 

 

As discussed, I was not able to reproduce the first behavior even if I uncheck "Delete previously generated files".

MahmoudBenRomdhane_0-1768816430862.png

MahmoudBenRomdhane_1-1768816565463.png

The second issue is confirmed and a child ticked is reported to the dedicated team. (Ticket Number: 225397)

I will let you know when the issue is solved.

 

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

ST Technical Moderator
January 14, 2026

Hello @matteverze 

Let me thank you for posting.

Could you provide please your Ioc.File.

Thanks

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
January 14, 2026

Hi @Mahmoud Ben Romdhane,

here it is. I see that the problem happened if I click on the "Migrate" option.

Thanks

ST Technical Moderator
January 19, 2026

Hello @matteverze 

 

As discussed, I was not able to reproduce the first behavior even if I uncheck "Delete previously generated files".

MahmoudBenRomdhane_0-1768816430862.png

MahmoudBenRomdhane_1-1768816565463.png

The second issue is confirmed and a child ticked is reported to the dedicated team. (Ticket Number: 225397)

I will let you know when the issue is solved.

 

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.