Skip to main content
AGoro.1
Associate
Jun 18, 2020 9:23 AM UTC
Solved

STM32Cube NUCLEO-F413ZH UART missing

Hello,

I am trying to create a project with STM32Cube 5.1.0 for NUCLEO-F413ZH. I see only USART 1, 2, 3 and 6 available, none of the UARTs 4, 5, 7, 8, 9 and 10. These UARTs are available if I open a project for STM32F413ZHT, the device used in NUCLEO-F413ZH board. I understand why UART4 would be disabled - its pins PA0/1 are used for other functions in NUCLEO, a user button and RMII_REF_CLK, but UART7 PH6/7 is not occupied.

Thank you.

This topic has been closed for replies.
berendi
berendiBest answer
Principal
Jun 18, 2020 9:33 AM UTC

Update CubeMX, the current version is 5.6.1.

STM32F413 has no ethernet interface.

2 replies

berendi
berendiBest answer
Principal
Jun 18, 2020 9:33 AM UTC

Update CubeMX, the current version is 5.6.1.

STM32F413 has no ethernet interface.

AGoro.1
AGoro.1Author
Associate
Jun 24, 2020 8:59 AM UTC

Thank you. In version 5.6.1 all UART are available.

NUCLEO-F413 has not Ethernet, but the GPIO are still reserved for other MCUs.