Skip to main content
rbenesh
Associate II
Aug 19, 2015 7:12 PM UTC
Question

STM32Cube_FW_F0_V1.2 versus 1.3

Posted on August 19, 2015 at 21:12

It is becoming annoying that since ST's inception of a Cortex implementation there have been Standard Peripheral libraries that simply are not standards to rely on.

I thought that switching to the HAL libraries would eliminate unnecessary changes but, yet again I am proven wrong.

This time it is macro names that have changed between libraries.

1.2 had.......                                     1.3 now has..........

  __APB1_FORCE_RESET();     __HAL_RCC_APB1_FORCE_RESET();

 __GPIOx_CLK_ENABLE();      __HAL_RCC_GPIOx_CLK_ENABLE();

.......etc. et cetera

After switching from the old 1.2.0 HAL to the new 1.3.0 hoping the update would fix the multitude of UART issues; I find that I now have to go back and change anything that used a macro in my code to add ''__HAL_RCC_'' in front of it. Why? Why were the macro names changed?

Who at ST needed something to do that they felt like changing unnecessarily the names on macros?

If you are going to standardize a library; correct items within a function \ macro, add new functions or add more macros; STOP changing names of macros!!!!!!

#hal #stm32cubemx #cubemx
This topic has been closed for replies.

3 replies

Nickname5522_O
Visitor II
Aug 20, 2015 10:36 AM UTC
Posted on August 20, 2015 at 12:36

Hi NStuff,

1-You don't need to change macro's name by adding ''__HAL_RCC_'', you have only to include the file ''stm32_hal_legacy.h'' in the main.c.

2-Who at ST needed something to do that they felt like changing unnecessarily the names on macros?

 

The reason of this change is to ensure that all series' drivers are compatible, so the user is able to migrate from one serie to another without trouble.

-Shahrzad- 
rbenesh
rbeneshAuthor
Associate II
Aug 21, 2015 2:16 AM UTC
Posted on August 21, 2015 at 04:16

As long as there is an upwards path; this should work. Is the legacy file documented?

Also, in the past there were migration documents from standard peripheral library x to y. Is there a document for converting from the standard peripheral library to the HAL?

Nickname5522_O
Visitor II
Aug 21, 2015 10:11 AM UTC
Posted on August 21, 2015 at 12:11

Hi NStuff,

-Under the Release_Notes file (STM32Cube_FW_F4_V1.7.0\Drivers\STM32F4xx_HAL_Driver),  there is a note concerning the addition of

stm32_hal_legacy.h. 

Concerning F0 package, it is not mentioned. We apologize for any inconvenience caused and an enhancement has been reported.

-Also thers is no document related to the migration from Standard Peripheral Library to HAL drivers.

-Shahrzad- 

As long as there is an upwards path; this should work. Is the legacy file documented?

Also, in the past there were migration documents from standard peripheral library x to y. Is there a document for converting from the standard peripheral library to the HAL?