Skip to main content
Associate
Mar 11, 2026 12:57 PM UTC
Solved

STM32_WPAN not possible to build without adv_trace and UART peripheral enabled

I'm trying to configure and generate a project with STM32CubeMX for the STM32WBA5MMGHx BLE module.

When enabling the STM32_WPAN middleware, the ADV_TRACE module gets automatically enabled under Utilities. This in turn requires to enable at least one UART/LPUART peripheral, otherwise type UART_HandleTypeDef is undefined and compiler throws and error:

../../Core/Inc/app_conf.h:304:8: error: unknown type name 'UART_HandleTypeDef'; did you mean 'RTC_HandleTypeDef'?
[build] 304 | extern UART_HandleTypeDef huart1;
[build] | ^~~~~~~~~~~~~~~~~~
[build] | RTC_HandleTypeDef

The STM32_WPAN throws a warning about not configured/wrong Platform Settings.

Is there any possibility to configure STM32_WPAN without ADV_TRACE enabled?

Used STM32CubeMX version is 6.17.0 and WBA firmware v1.19.0 and cmake project is generated.

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Jul 1, 2026 8:22 AM UTC

Hello ​@Lix Paulian  

You are right. the issue still occurs in STM32CubeMX 6.18.0 

 the following ticket has been escalated to dev team #0064182 in order to double check this issue.

BR,

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

9 replies

Associate
Mar 24, 2026 4:27 PM UTC

Hi,

I’m sorry to bother you, but I am currently facing a very similar issue.

I am working on a project based on the STM32WBA65, using the BLE stack along with the sequencer (UTIL_SEQ). I started from the BLE_DataThroughput example provided by ST and I am adapting it to my custom hardware.

However, my board does not include any UART peripheral, and I do not need any UART-based debug or trace functionality.

The problem is that CubeMX forces the ADV_TRACE middleware to remain enabled when BLE is activated. As a result, the project depends on UART (for example UART_HandleTypeDef huart1), which leads to compilation errors such as:

unknown type name 'UART_HandleTypeDef'

This seems very similar to the issue you described.

Have you made any progress on this topic or found a clean workaround to remove the UART dependency?

I would be very interested in any suggestions or best practices.

Thank you in advance!

Best regards,
Pierre

 

Andrew Neil
Super User
Mar 24, 2026 4:58 PM UTC

@christianegerer wrote:

otherwise type UART_HandleTypeDef is undefined and compiler throws an error:.


Have you checked to see if there's any #if which should be disabling that line?

If that's the only error, then a workaround would be to just delete or comment-out that line.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
Mar 25, 2026 7:21 AM UTC

@Andrew Neil : the part of the code is auto-generated by CubeMX. Of course a workaround is to manually delete/comment this line after each code regeneration. It's just annoying. Additionally, at least for CMake based project, CubeMX adds the file adv_trace_usart_if.c  to the target sources in the auto-generated cmake/stm32cubemx/CMakeLists.txt file. So if you comment out the line

extern UART_HandleTypeDef huart1;

in app_conf.h, you also need to remove adv_trace_usart_if.c from the target sources by doing something like this in the root CMakeLists.txt:

get_target_property(COMMON_SRC Common SOURCES)
list(REMOVE_ITEM COMMON_SRC ${CMAKE_CURRENT_SOURCE_DIR}/cmake/stm32cubemx/../../Projects/Common/WPAN/Interfaces/adv_trace_usart_if.c)
set_target_properties(Common PROPERTIES SOURCES "${COMMON_SRC}")

Otherwise, you get more compile errors in adv_trace_usart_if.c. Don't know if a similar workaround is possible for the Eclipse-based CubeIDE.

Actually, it would be nice if CubeMX would allow a custom logging backend besides UART. I actually replaced now adv_trace_usart_if.c with a custom adv_trace_rtt_if.c to log via Segger RTT. But it still requires to define a UART peripheral in CubeMX because of this line above in app_conf.h. Fortunately, I have the spare pins available to define a LPUART peripheral on my custom board although I don't use it.

@Pierre_Agneray : If you can afford it, i.e., if you have spare pins on your custom board, you can just enable a UART/LPUART in CubeMX as the easiest workaround. If not, I think you need to manually modify the auto-generated sources. Maybe it can be even automated. Haven't tried that except for the CMake part in my setup.

Anyway, to me it looks like a logical error in the auto-generated sources by CubeMX and I hope ST fixes this in an upcoming release (and maybe even allows custom logging backends).

Associate
Mar 25, 2026 8:15 AM UTC

@christianegerer  Thank you very much for your detailed answer.

Enabling a UART/LPUART peripheral does indeed fix the issue on my side, so I will use this workaround for initial testing.

However, I will eventually need to remove the UART in the final version of my project, as I am working on a low-power system. Keeping an unused UART enabled could negatively impact power consumption, which I would like to avoid.

@Andrew Neil You are right, manually deleting or commenting out the generated code is a possible workaround. However, in practice it quickly becomes quite tedious, as the UART introduces multiple dependencies across many generated files

@christianegerer I also find your idea of automating the cleanup process very interesting. I may try to write a small Python script to remove the unwanted files and references after code generation, although this also adds some complexity to the workflow

In any case, this does seem like a limitation (or inconsistency) in the current CubeMX code generation, and I hope it will be improved in a future release.

Thank you all for your help and insights.

Best regards,
Pierre

ST Technical Moderator
Mar 29, 2026 4:53 PM UTC

Hello All,

I will inform our CubeMX team about this related request and your feedback.

@Ghofrane GSOURI Could you please review this post.

Thank you for your contribution.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Lix Paulian
Associate II
Jun 17, 2026 3:16 PM UTC

Hello, I have the same issue, and I cannot use the workarounds found here, because I have no pins to give: as I am using the small chip (UFQFPN32), the two pins of the UART are very precious to me. I don’t understand why one cannot unclick in the CubeMX the “ADV_TRACE” utility, because not everybody uses it. I am using for tracing the Segger J-Link over ITC, for example. This seems as a nasty bug to me.

I hope for an CubeMX update as soon as possible.

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Jul 1, 2026 8:22 AM UTC

Hello ​@Lix Paulian  

You are right. the issue still occurs in STM32CubeMX 6.18.0 

 the following ticket has been escalated to dev team #0064182 in order to double check this issue.

BR,

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Lix Paulian
Associate II
Jul 8, 2026 8:24 AM UTC

Hello Ghofrane,

I can’t see how the issue has been solved, I installed CubeMX 6.18.0 but I still can’t get rid of ADV_TRACE after enabling the STM32_WPAN middleware. Is there a special trick I don’t know?