Skip to main content
VSerb.1
Visitor II
Oct 6, 2022 5:20 PM UTC
Question

STM32 USB HS DMA stuck

Hello.

I try to setup CDC USB HS with DMA but it blocks after few samples sent.

Here is the minimal code that replicate the problem

int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USB_DEVICE_Init();
 /* USER CODE BEGIN 2 */
 
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 int32_t ssss=0;
 char msg2[2048];
 while (1)
 {
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 
	 sprintf(msg2, "%d\r\n", ssss);
	 CDC_Transmit_HS((uint8_t *) msg2, strlen(msg2));
	 ssss++;
	 HAL_Delay(10);
 }
 /* USER CODE END 3 */
}

On the host side, I open CDC com port in putty, I begin to receive samples sents by stm32 but immediately after few sample no more lines appears.

0693W00000UnWheQAF.png...

0693W00000UnWhtQAF.pngIt blocks here with USBD_BUSY:

0693W00000UnWjpQAF.pngI use STM32F769I-DISCO board,

STM32CubeMX Version 6.6.1

STM32Cube FW_F7 V1.17.0

CPU ICache and DCache disabled

Log output file: c:\users\victors\appdata\local\temp\stm32cubeprogrammer_a14036.log
ST-LINK SN : 0671FF555071494867091122
ST-LINK FW : V2J39M27
Board : 32F769IDISCOVERY
Voltage : 3.21V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x451
Revision ID : Rev Z
Device name : STM32F76x/STM32F77x
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : --
 
 
 
Memory Programming ...
Opening and parsing file: st-link_gdb_server_a14036.srec
 File : st-link_gdb_server_a14036.srec
 Size : 33.41 KB 
 Address : 0x08000000 
 
 
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 1]
Download in Progress:

0693W00000UnWirQAF.png 

0693W00000UnWiwQAF.png0693W00000UnWj6QAF.png0693W00000UnWjBQAV.png 

If I set Enable internal IP DMA for USB_OTG_HS to disabled it works without stopping.

Could you please take a look?

Thanks

This topic has been closed for replies.

2 replies

TianZhang
Visitor II
Jan 7, 2023 9:51 PM UTC

Hi

I'm using OTG HS on the STM32F746 mcu, in device mode, as a CDC VCP. It works when "Internal IP DMA" is disabled. If I enable DMA, the USB device enumerates but CDC_Transmit_HS() no longer works.

Please let me know the solution if you have solved already.

Best regards,

Tian.

bhaskarm
Associate
Apr 27, 2023 12:10 AM UTC

Can you take a look at this issue and tell me if it solves your problem?

Problem with STM32H747 HS USB DMA.