Skip to main content
Associate
August 1, 2024
Question

STM32 Cube MX and IAR

Hi All, 

I am trying to run a code with NUCLEO-U575ZI-Q The tool chain/ IDE is  EWARM but the unable to select the latest version of IAR(9.50) The option is available only until IAR version 8.5. When I select generate code and select open project the IAR version 8.5 IDE opens and I will not be able to debug the firmware

I am able to debug the run the firmware  when I select open folder  and run EWARM from latest version of IAR(9.50)

Is there a way to be able to see the latest version on STM Cube MX  ?

This topic has been closed for replies.

2 replies

TDK
August 1, 2024

Probably just isn't supported yet.

v8.50 is the latest supported version per the release notes.

rn0094-stm32cubemx-release-6120-stmicroelectronics.pdf

 

Surely you can open up projects created for v8.5 in newer versions. All IDEs have good backwards compatibility support, especially for the last few versions.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Pavel A.
August 1, 2024

Open the project in the latest IAR 9.x and upgrade it (the project) when prompted.