Skip to main content
predrag10
Associate II
Aug 23, 2014 8:14 AM UTC
Question

STM32 Cube for F1 devices

Posted on August 23, 2014 at 10:14

Does somebody know when the F1 devices will be completely supported on STM32 Cube(i.e. STM32F103)?

#stmcube-stmcubemx #stm32f1
This topic has been closed for replies.

7 replies

Montassar BEN ROMDHANE_O
Visitor II
Sep 5, 2014 2:17 PM UTC
Posted on September 05, 2014 at 16:17

Hi pejic.predrag.001,

The STM32CubeF1 release target is very end of year.

Thank you for your interest in our STM32Cube solution.

With regards.

bernieserver
Associate II
Dec 1, 2014 12:07 PM UTC
Posted on December 01, 2014 at 13:07

Hello Heisenberg,

are there any news about the release date for full support of F1 devices in CubeMX?

I.E: STM32F103ZG?

Thank you!

Regards

Bernhard

kujawa
Visitor II
Dec 7, 2014 12:51 PM UTC
Posted on December 07, 2014 at 13:51

Hi. I also very wait for F1 support. Maybe some BETA version is available.

bernieserver
Associate II
Dec 8, 2014 12:35 PM UTC
Posted on December 08, 2014 at 13:35

Hi,

any new updates about F1 release?

uc2013135191
Associate III
Dec 17, 2014 5:32 PM UTC
Posted on December 17, 2014 at 18:32

I also would like to know if there is any updates on the release.

I don't want to go learning to use the older std. library since when i start to work (still studying) the stm32cube will be more mature (and looks promissing so far).

uilyas
Visitor II
Jan 6, 2015 6:42 AM UTC
Posted on January 06, 2015 at 07:42

Any update on Cube for F1 family ?

waiting...

gw_it
Associate III
Jan 15, 2015 2:21 PM UTC
Posted on January 15, 2015 at 15:21

Here too, I have some software that I use on both F103 and F401 parts.

It was bad enough having two separate libraries with subtly different names, but now I've got the STM32 cube libs for the F401 part and the old libraries for the F103, suddenly all the function names for one device are pointlessly prefixed with 'HAL_' and on the other device they're not. It makes sharing code pretty much impossible.