Skip to main content
Visitor II
July 20, 2023
Question

STM32- Can not initialize eMMC, CMDTIMEOUT

I have problem with using stm32 drivers for connection to eMMC.https://datasheet.lcsc.com/lcsc/2205071500_Zetta-ZDEMMC04GA_C3010207.pdf

Problem is that the initialization pop up error, because timeout occures in function static uint32_t SDMMC_GetCmdError(SDIO_TypeDef *SDIOx). I'm using sdio MMC 4bus connection. With default configuration generated with cube MX. Whole CubeIDE project: https://drive.google.com/file/d/17Y-EmB60kiUhar9B0o4DANVTT_GUKXUu/view?usp=drive_link

INITIALIZATION FUNCTION:

static void SDIO_MMC_Init(void){
 hmmc.Instance = SDIO;
 hmmc.Init.ClockEdge = SDIO_CLOCK_EDGE_RISING;
 hmmc.Init.ClockBypass = SDIO_CLOCK_BYPASS_DISABLE;
 hmmc.Init.ClockPowerSave = SDIO_CLOCK_POWER_SAVE_DISABLE;
 hmmc.Init.BusWide = SDIO_BUS_WIDE_4B;
 hmmc.Init.HardwareFlowControl = SDIO_HARDWARE_FLOW_CONTROL_DISABLE;
 hmmc.Init.ClockDiv = 0;
 if (HAL_MMC_Init(&hmmc) != HAL_OK){
 Error_Handler();
 }
 if (HAL_MMC_ConfigWideBusOperation(&hmmc, SDIO_BUS_WIDE_4B) != HAL_OK){
 Error_Handler();
 }
 
 }

MSP_INITIALIZATION

void HAL_MMC_MspInit(MMC_HandleTypeDef* hmmc)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 if(hmmc->Instance==SDIO)
 {
 /* USER CODE BEGIN SDIO_MspInit 0 */

 /* USER CODE END SDIO_MspInit 0 */
 /* Peripheral clock enable */
 __HAL_RCC_SDIO_CLK_ENABLE();

 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();
 /**SDIO GPIO Configuration
 PC8 ------> SDIO_D0
 PC9 ------> SDIO_D1
 PC10 ------> SDIO_D2
 PC11 ------> SDIO_D3
 PC12 ------> SDIO_CK
 PD2 ------> SDIO_CMD
 */
 GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10|GPIO_PIN_11
 |GPIO_PIN_12;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF12_SDIO;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 GPIO_InitStruct.Pin = GPIO_PIN_2;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF12_SDIO;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 /* USER CODE BEGIN SDIO_MspInit 1 */

 /* USER CODE END SDIO_MspInit 1 */
 }
}

 

    This topic has been closed for replies.

    1 reply

    Ghofrane GSOURI
    ST Technical Moderator
    July 21, 2023

    Hello @Trahery 

    First let me thank you for reporting.

    The function SDMMC_GetCmdError() is used to get the command error flags from the SDIO peripheral after a command has been sent to the eMMC card. The function returns a 32-bit value that represents the error flags for the last command that was sent.

    If a pop-up error occurs in this function, it usually indicates that there was an error during the command transmission or response processing. This could be due to a variety of reasons, such as incorrect command parameters, improper initialization of the SDIO peripheral, or communication errors with the eMMC card itself.

    To resolve the issue, you can try the following:

    1. Check the command parameters and ensure that they are correct for the eMMC card being used.

    2. Verify that the SDIO peripheral is properly initialized and configured for the eMMC card.

    3. Check the communication lines between the MCU and the eMMC card to ensure that there are no issues with the physical connection.

    4. Try using a different eMMC card to see if the issue is related to the card itself.

    5. Increase the timeout value for the command response to see if that resolves the issue.

    6. Check the SDIO interrupt status registers to see if there are any errors or interrupts that are being generated during the command transmission.

    Thx

    Ghofrane

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.