Skip to main content
Professional
Associate III
Aug 31, 2018 12:22 PM UTC
Question

STM32 + ADC Dual regular simultaneous mode and DMA : need to call HAL_DMA_Init

Hello,

i want to use 3 ADC :

-ADC1 et ADC2 in Dual regular simultaneous mode + trigger on timer +DMA

-ADC3 on its own in continuous mode + DMA.

According to reference manuel,for DMA :

-ADC1 can use channel0 + stream0

-ADC2 can use channel1 + stream2

-ADC3 can use channel2 + stream1

Is it mandatory to program explicitely the DMA ? (cubemx doesn't call  HAL_DMA_Init function)

Do i need to do the following initialization :

g_DmaHandleADC1.Instance = DMA2_Stream0;

 g_DmaHandleADC1.Init.Channel = DMA_CHANNEL_0;

 g_DmaHandleADC1.Init.Direction = DMA_PERIPH_TO_MEMORY;

 g_DmaHandleADC1.Init.PeriphInc = DMA_PINC_DISABLE;

 g_DmaHandleADC1.Init.MemInc = DMA_MINC_ENABLE;

 g_DmaHandleADC1.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;

 g_DmaHandleADC1.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;

 g_DmaHandleADC1.Init.Mode = DMA_NORMAL; //DMA_CIRCULAR;

 g_DmaHandleADC1.Init.Priority = DMA_PRIORITY_HIGH;

 g_DmaHandleADC1.Init.FIFOMode = DMA_FIFOMODE_DISABLE;

 g_DmaHandleADC1.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_HALFFULL;

 g_DmaHandleADC1.Init.MemBurst = DMA_MBURST_SINGLE;

 g_DmaHandleADC1.Init.PeriphBurst = DMA_PBURST_SINGLE;

 HAL_DMA_Init(&g_DmaHandleADC1);

 __HAL_LINKDMA(&hadc1, DMA_Handle, g_DmaHandleADC1);

 g_DmaHandleADC2.Instance = DMA2_Stream0;

 g_DmaHandleADC2.Init.Channel = DMA_CHANNEL_2;

 g_DmaHandleADC2.Init.Direction = DMA_PERIPH_TO_MEMORY;

 g_DmaHandleADC2.Init.PeriphInc = DMA_PINC_DISABLE;

 g_DmaHandleADC2.Init.MemInc = DMA_MINC_ENABLE;

 g_DmaHandleADC2.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;

 g_DmaHandleADC2.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;

 g_DmaHandleADC2.Init.Mode =DMA_NORMAL; //DMA_CIRCULAR;

 g_DmaHandleADC2.Init.Priority = DMA_PRIORITY_HIGH;

 g_DmaHandleADC2.Init.FIFOMode = DMA_FIFOMODE_DISABLE;

 g_DmaHandleADC2.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_HALFFULL;

 g_DmaHandleADC2.Init.MemBurst = DMA_MBURST_SINGLE;

 g_DmaHandleADC2.Init.PeriphBurst = DMA_PBURST_SINGLE;

 HAL_DMA_Init(&g_DmaHandleADC2);

 __HAL_LINKDMA(&hadc2, DMA_Handle, g_DmaHandleADC2);

 g_DmaHandleADC3.Instance = DMA2_Stream0;

 g_DmaHandleADC3.Init.Channel = DMA_CHANNEL_1;

 g_DmaHandleADC3.Init.Direction = DMA_PERIPH_TO_MEMORY;

 g_DmaHandleADC3.Init.PeriphInc = DMA_PINC_DISABLE;

 g_DmaHandleADC3.Init.MemInc = DMA_MINC_ENABLE;

 g_DmaHandleADC3.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;

 g_DmaHandleADC3.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;

 g_DmaHandleADC3.Init.Mode = DMA_NORMAL; //DMA_CIRCULAR;

 g_DmaHandleADC3.Init.Priority = DMA_PRIORITY_HIGH;

 g_DmaHandleADC3.Init.FIFOMode = DMA_FIFOMODE_DISABLE;

 g_DmaHandleADC3.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_HALFFULL;

 g_DmaHandleADC3.Init.MemBurst = DMA_MBURST_SINGLE;

 g_DmaHandleADC3.Init.PeriphBurst = DMA_PBURST_SINGLE;

 HAL_DMA_Init(&g_DmaHandleADC3);

 __HAL_LINKDMA(&hadc3, DMA_Handle, g_DmaHandleADC3);

best regards

thanks

This topic has been closed for replies.

2 replies

Amel NASRI
ST Technical Moderator
Sep 18, 2018 8:56 AM UTC

Hi @Professional​ ,

You need to configure DMA in STM32CubeMX, then the initialization code for DMA will be added.

You need to check both main.c file as well as the generated stm32xxxx_hal_msp.c file.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Professional
Associate III
Sep 21, 2018 1:29 PM UTC

Hello

thank you very much for your reply : i was just looking at main.c

I have programmed ADC1 + ADC2 in Dual regular simultaneous mode and continuous mode, and i validated DMA2 stream0 and stream2 global interrupt in CubeMX

1) If i call the  HAL_ADC_Start_DMA (&hadc1, (uint32_t *) &aADCxConvertedData[0], ADC_CONVERTED_DATA_BUFFER_SIZE );

will it start the ADC1 and ADC2 in continuous mode (has just handle for ADC1 is given) ?

2) in the function void DMA2_Stream0_IRQHandler() can i get the data from ADC1 conversion (in aADCxConvertedData array)

3) in the function void DMA2_Stream2_IRQHandler() can i get the data from ADC2 conversion : where are they placed in my aADCxConvertedData array ?

thanks

regards