[ST Edge AI Core v4.1.0 / NUCLEO-U3C5ZI-Q] Online CubeMX template still serves STM32Cube_FW_U3 v1.4.0 instead of v1.5.0
Hello ST team—when running on-target validation on a NUCLEO-U3C5ZI-Q board (STM32U3C5, Cortex-M33, TrustZone disabled) with ST Edge AI Core v4.1.0 and HSP acceleration enabled, our INT8 ONNX model hangs during inference and hits a 50-second serial read timeout, whereas CPU-only validation passes. The generation logs show that selecting this target downloads an online CubeMX template packaged with STM32Cube_FW_U3 firmware version 1.4.0, even though the ST Edge AI Core v4.1.0 release notes state that firmware v1.5.0 or newer is required for HSP support on STM32U3Cxx devices. Could you please update the online template service for the NUCLEO-U3C5ZI-Q to STM32Cube_FW_U3 v1.5.0 or later, and let us know if there is a supported way in the meantime to make STM32Cube AI Studio use a locally installed v1.5.0 firmware package instead of fetching the v1.4.0 online template?