Skip to main content
bugiii
Associate
Oct 16, 2019 3:23 PM UTC
Solved

[SOLVED] STM32CubeMX does not properly generate files for STM32CubeIDE.

I am using SW4STM32 as the toolchain in STM32CubeMX v5.4.0. The MCU I am using is the STM32H7 series.

In order to transfer Toolchain to STM32CubeIDE v.1.1.0, like SW4STM32, STM32CubeIDE was selected in Toolchain and GENERATE CODE button was pressed.

However, only Core and Driver codes are generated regardless of whether or not Generate Under Root is checked. Project files (.project, .cproject), .ld files, and startup code are not generated.

As with other similar questions ( https://community.st.com/s/question/0D50X0000AlcdBSSQY/stm32cubeide-cant-compile-stm32cubemx-520-projects-for-stm32cubeide?t=1571237740185 ), I uninstalled Java and MX and did a fresh install with the 64-bit version, but that didn't fix the problem.

Please let me know if there is a solution.

This topic has been closed for replies.
bugiii
bugiiiBest answer
Associate
Oct 19, 2019 11:22 PM UTC

After a completely new installation of Windows 10 and an offline Java 64-bit version, I installed CubeMX v5.4.0 and it worked fine.

On machines that already have MX v5.3.0 installed, the following worked fine:

1. Uninstall Java completely and install the offline 64-bit version.

2. Do not update inside MX v5.3.0, uninstall v5.3.0 completely and install v5.4.0.

3 replies

Cartu38 OpenDev
Graduate II
Oct 18, 2019 5:51 AM UTC

Maybe some weird metadata preventing you to succeed ? Could you have a try to remove <user>/.stm32cubeide folder and get a new try ?

bugiii
bugiiiAuthor
Associate
Oct 19, 2019 12:57 AM UTC

I tried removing all the .stm32cubeide directories on the disk, but with the same result.

bugiii
bugiiiAuthorBest answer
Associate
Oct 19, 2019 11:22 PM UTC

After a completely new installation of Windows 10 and an offline Java 64-bit version, I installed CubeMX v5.4.0 and it worked fine.

On machines that already have MX v5.3.0 installed, the following worked fine:

1. Uninstall Java completely and install the offline 64-bit version.

2. Do not update inside MX v5.3.0, uninstall v5.3.0 completely and install v5.4.0.