Skip to main content
G_1
Associate
Apr 8, 2019 2:43 PM UTC
Question

SOLVED: CubeMX 5.1.0 re-generated project for SW4STM32 linker script *.LD file is empty. GONE: with CubeMX 5.2

CubeMX 5.1.0 and STM32F302 every time a project is re-generated the

STM32F302R8Tx_FLASH.ld file is empty.

This topic has been closed for replies.

19 replies

Nesrine.JLASSI
Visitor II
Apr 24, 2019 2:22 PM UTC
Mark Shoe
Associate III
May 10, 2019 7:19 AM UTC

This happens me many times on different cpu's. The empty file problem started from version 5.1.0.

It is a problem for me because I made changes to the sections for the bootloader.

Nesrine.JLASSI
Visitor II
May 10, 2019 7:45 AM UTC

Hi @Community member​ 

This is a bug that has been fixed in the new version of STM32CubeMX 5.2.0.

Best regards,

Nesrine

Rutr
Visitor II
Jun 27, 2019 6:26 PM UTC

Also I and my friends have this problem. Cube eclipse plugin version 5.1.0.

After re-geneerate the linker file is empty. STM32 F103C8, Windows 10 x64

Is there cube eclipse plugin in version 5.2 ?

G_1
G_1Author
Associate
Jun 28, 2019 6:17 AM UTC

Hi,

use 5.2 and the error is gone.

There are three ways to get the update.

Nice day and regards.

G_1
G_1Author
Associate
Jun 28, 2019 6:18 AM UTC

Hi

use 5.2 and the error is gone. There are three ways to do the update.

So long and THX