Skip to main content
Associate
June 15, 2026
Question

Should the Init_Debug() function be called for the SED thread's low-power operation?

  • June 15, 2026
  • 0 replies
  • 16 views

Hello.

I am building a Thread SED product using the STM32W5MMG.

 

Recently, after upgrading the firmware version to v1.24.0, I encountered a problem with low-power startup.

Upon investigation, I discovered that the location of the “Init_Debug();” call within the MX_APPE_Init() method in app_entry.c was different.

Previously (in v1.23.0), I had written the following code within the /* USER CODE BEGIN APPE_Init_1 */ block, and this worked correctly.


HW_TS_Init(hw_ts_InitMode_Full, &hrtc); /**< Initialize the TimerServer */

/* USER CODE BEGIN APPE_Init_1 */
#if (CFG_FULL_LOW_POWER != 1)
Init_Debug();
#endif

UTIL_LPM_SetStopMode(1 << CFG_LPM_APP, UTIL_LPM_DISABLE);
UTIL_LPM_SetOffMode(1 << CFG_LPM_APP, UTIL_LPM_DISABLE);

Led_Init();
Button_Init();
/* USER CODE END APPE_Init_1 */

 

 However, with the transition to v1.24.0, the call location of Init_Debug(); was changed as follows.


HW_TS_Init(hw_ts_InitMode_Full, &hrtc); /**< Initialize the TimerServer */

Init_Debug();
/* USER CODE BEGIN APPE_Init_1 */

UTIL_LPM_SetStopMode(1 << CFG_LPM_APP, UTIL_LPM_DISABLE);
UTIL_LPM_SetOffMode(1 << CFG_LPM_APP, UTIL_LPM_DISABLE);

Led_Init();
Button_Init();
/* USER CODE END APPE_Init_1 */

So, from now on, even if CFG_FULL_LOW_POWER is set to enabled in CubeMX, Init_Debug() must be called.

But in this case, my system freezes somewhere I don't know and does not enter low power mode also.

So I have to manually comment out the Init_Debug() call to solve this problem.

 

I don’t think this way is a good way.

I wonder if I need to artificially block Init_Debug calls to ensure my product works from now on, or if there is another pitfall I am missing.

 

Thanks,