Skip to main content
Luiz Pereira
Associate II
July 15, 2023
Question

Serious bug in CubeMX 6.9.0 ??

The new version of CubeMX (6.9.0) no mater of options in Project Manager / Code Generator, if  Keil Toolchain / IDE is choosen, the project regeneration delete the previous .uvprojx file and generates a new one, LOOSING ALL changes made by the user in the project. For now, I uninstalled the new version and went back to the previous one (6.8.1). Any solutions I haven't seen?

Meanwhile, I continue with the aforementioned problem (CubeMX messed up) and there is no way to solve it (I'm honestly disappointed...)

This topic has been closed for replies.

3 replies

Ghofrane GSOURI
ST Technical Moderator
July 17, 2023

Hello @Luiz Pereira 


Thank you for having reported.


I assume this is the exact same issue already reported to the development team and tracked by the Ticket 157222  and that will be fixed as soon as possible.

The issue is detected only when you use keil Toolchain , in the other hand STM32CubeIDE 1.13.0 and EWARM work correctly : they do not delete the added user file after regeneration.

Thx

Ghofrane

 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Luiz Pereira
Associate II
July 18, 2023

Hi @Ghofrane GSOURI 

Thanks for the update. It is effectievlly the issue reported. I will wait for news. 

BTW, is there any explanation for the problem (and I saw that it has also been reported but without solution) with CubeMX's UI interface?

Thanks again

Luiz

Jnevi.1
Associate III
July 18, 2023

can confirm this. should have checked here before updating.
everytime after i update cubemx or touchgfx different things are broken :\