Skip to main content
fredferd
Associate II
Feb 26, 2019 7:54 PM UTC
Question

SDMMC: auto card detect?

In CubeMX when choosing fatfs middleware it seems to require a gpio pin. Is that just a limitation in CubeMX?

Basically is there a reliable software card detect mechanism using the existing SDMMC lines (4 pin SD card) or must an extra gpio pin be used to the sd card detect pin?

Thanks,

-Fred

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Feb 26, 2019 9:09 PM UTC

As the sockets pretty much all have a mechanical switch mechanism, people tend to focus on those. ST has some of their board examples use that to generate an EXTI interrupt.

The example code is mostly provided as a demo of functionality, not something that would meet commercial requirements for fit/finish.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..