Skip to main content
YFric
Associate II
Jan 5, 2019 8:21 PM UTC
Question

SDIO problem when using FatFS on STM32F413

Hi, I am currently working on a project where I will have to log data to an µSD card using a STM32F413. I created a project in STM32CubeMX (version 5.0.0) and setup SDIO (currently in SD 1bit mode, but I also tried 4 bit mode). I also set up FatFS in CubeMX. After generating the code and trying to mount the sd card:

FRESULT mountresult = f_mount(&SDFatFS, "", 1);
	if(mountresult == FR_OK)
	{
 
	}
	else{
		HAL_GPIO_TogglePin(LED4_GPIO_Port,LED4_Pin);
		if(mountresult == FR_NOT_READY){
			HAL_GPIO_WritePin(LED2_GPIO_Port,LED2_Pin,GPIO_PIN_SET);
		}
 
	}

LED 2 and 4 light up, meaning that the result was FR_NOT_READY.

After digging deeper I find the problem situates at the BSP_SD_Init(void) function,

here HAL_SD_Init(SD_HandleTypeDef *hsd) is called,

in this function HAL_SD_InitCard(SD_HandleTypeDef *hsd) is called,

at last SD_PowerON(hsd); is called

finally the error situates here: (lines 2560-2565 in stm32f4xx_hal_sd.c)

/* SEND CMD55 APP_CMD with RCA as 0 */
errorstate = SDMMC_CmdAppCommand(hsd->Instance, 0U);
if(errorstate != HAL_SD_ERROR_NONE)
{
 return HAL_SD_ERROR_UNSUPPORTED_FEATURE;
}

The SDMMC_CmdAppCommand returns an error state, meaning that it is 'an unsupported feature'. However I can't find what the meaning of this error is and how I would be able to fix it.

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
Jan 5, 2019 10:09 PM UTC

Is this a 1GB or less sized card?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
YFric
YFricAuthor
Associate II
Jan 5, 2019 10:11 PM UTC

No, it is a 8GB SDHC card from Kingston

YFric
YFricAuthor
Associate II
Jan 9, 2019 6:31 PM UTC

I fixed the problem, I had to add SDIO DMA streams since these are used by default

Curtis B.
Associate III
Oct 1, 2019 10:50 AM UTC

Hi,

currently I am facing the same problem. I manually added the DMA streams in the CubeMX GUI. Unfortunately, this didn't solve the problem. Anyway, I do not see, why adding DMA streams should help at this point, as these streams are used for the read and write block functions. If I understood the code correctly, the SDIO interface directly sends commands and watches for some flags to evaluate during this init sequence. Did you change any other things that might had an influence on that issue.

Best regards,

Daniel