Skip to main content
APapa.14
Associate
Apr 9, 2019 3:22 PM UTC
Question

[RTOS] osDelay stuck after passing argument in UART printf function

Hello !

My project works with FreeRTOS and HAL library (generate by CubeMX) on STM32L496 and I use TIM1 as timebase source instead of SystTick.

I have a problem with osDelay().

I have these functions to print what I want with an UART :

/* --------------------------------------------------------------------------*/
uint8_t	TUTxPutByte(uint8_t p_data)
{
 
	//Push character on UART
	return HAL_UART_Transmit(&huart3, &p_data, 1, 1);
 
 
}//end TUTxPutByte
/* --------------------------------------------------------------------------*/
 
 
/* --------------------------------------------------------------------------*/
uint8_t	sendMsg(char * p_msg_to_send, uint8_t p_CRLF)
{
	uint8_t	i = 0;					//Loop variable
	uint8_t	lengthMsg = 0;			//Length of ASCII data
	uint8_t	statusReturn = HAL_OK;	//Error function return
 
	//Calculate length of message
	lengthMsg = strlen(p_msg_to_send);
 
	//Transmit loop
	for(i = 0; i < lengthMsg; i++){
		//Send char by char with error control of HAL function
		if((statusReturn = TUTxPutByte(p_msg_to_send[i])) != HAL_OK)
		{
			return statusReturn;
		}
	}//end for
 
	//String termination
	if((p_CRLF == SEND_CR) || (p_CRLF == SEND_CR_LF))
	{
		//Send CR with error control of HAL function
		if((statusReturn = TUTxPutByte(0x0D)) != HAL_OK)	// [ASCII] CR
		{
			return statusReturn;
		}
	}
 
	//String termination
	if((p_CRLF == SEND_LF) || (p_CRLF == SEND_CR_LF))
	{
		//Send LF with error control of HAL function
		if((statusReturn = TUTxPutByte(0x0A)) != HAL_OK)	//< [ASCII] LF
		{
			return statusReturn;
		}
	}
 
	//Normal case
	return HAL_OK;
}//end sendMsg
/* --------------------------------------------------------------------------*/
 
/* --------------------------------------------------------------------------*/
uint8_t cprintf (const char *format, ...)
{
	uint8_t		i = 0;
	char		msg_to_write[SIZE_BUFFER_DEBUG] = {'\0'};	//Maximum 128 characters
 
	//Stack declaration
	va_list pile;
	//Last argument
	va_start(pile, format);
	//Array construction
	i = vsnprintf (msg_to_write, SIZE_BUFFER_DEBUG, format, pile);
 
	//Close stack
	va_end(pile);
 
	//Send Msg
	sendMsg(msg_to_write, NO_CR_LF);
 
	//Return number of characters sent
	return i;
}//end cprintf
/* --------------------------------------------------------------------------*/

When I use cprintf() function with a simple array (without arguments), all it works in my task, nothing stuck.

The problem is when I have an argument with cprintf as below:

void TestLOGTask(void const * argument)
{
 uint8_t value = 'a';
 for(;;)
 {
 cprintf("Value : %c\r\n", value);
 osDelay(250);
 }
}
 
void OtherTask(void const * argument)
{
 for(;;)
 {
 HAL_GPIO_WritePin(GPIOB, GPIO_PIN14, GPIO_PIN_SET);
 osDelay(250);
 HAL_GPIO_WritePin(GPIOB, GPIO_PIN14, GPIO_PIN_RESET);
 osDelay(250);
 }
}

osDelay stuck the runing execution in this configuration : it just execute one time my cprintf and stop execution of all task (including the blink led).

When I put HAL_Delay instead of osDelay() in TestLOGTask() OR/XOR OtherTask(), It works.

To resume :

  • Code works if no argument in cprintf
  • Code works if there is runing HAL_Delay at least in one task

Do you have any idea to solve this problem ?

Maybe due to mis-overwritting of the OS of tick function ?

This is strange because HAL_Delay just get tick, no set or init things.

Thank you in advance to any one who may be able to give me some ideas.

Adrian

This topic has been closed for replies.

2 replies

APapa.14
APapa.14Author
Associate
Apr 11, 2019 8:10 AM UTC

I solve this problem by increase the stack size of my task (use printf functions...).

However, I don't understand how it can works by using HAL_Delay() function.

coder.liss
Visitor II
Aug 31, 2019 1:23 PM UTC

I''m really appreciate your answer. I spent on it a whole day until I found your answer.