Skip to main content
SBhon.1
Associate II
Nov 8, 2022 6:19 AM UTC
Question

RTC reading wrong value on STM32L4

Hi. I am using STM32L412KB for my application and internal RTC for maintaining time. I get epoch time over UART and then I call the following function to set the time.

void set_rtc_time(time_t epoch_time)
{
 rtc_time = epoch_time;
 struct tm *time_sec = localtime(&epoch_time);
 RTC_TimeTypeDef time;
 time.Hours = (uint8_t)time_sec->tm_hour;
 time.Seconds = (uint8_t)time_sec->tm_sec;
 time.Minutes = (uint8_t)time_sec->tm_min;
 APP_ERROR_CHECK(HAL_RTC_SetTime(&hrtc, &time, RTC_FORMAT_BIN));
 RTC_DateTypeDef date;
 date.Date = (uint8_t)time_sec->tm_mday;
 date.Month = (uint8_t)time_sec->tm_mon + 1;
 date.Year = (uint8_t)time_sec->tm_year - 100;
 // date.WeekDay = time_sec->tm_wday;
 APP_ERROR_CHECK(HAL_RTC_SetDate(&hrtc, &date, RTC_FORMAT_BIN));
}

And after setting the time I respond back with the time set over UART. So, while creating the message to be transmitted over UART, I use following function to read the RTC and convert it to epoch time.

time_t get_rtc_epoch_time(void)
{
 RTC_TimeTypeDef rtc_time;
 RTC_DateTypeDef rtc_date;
 struct tm current_rtc_time;
 APP_ERROR_CHECK(HAL_RTC_GetTime(&hrtc, &rtc_time, RTC_FORMAT_BIN));
 APP_ERROR_CHECK(HAL_RTC_GetDate(&hrtc, &rtc_date, RTC_FORMAT_BIN));
 current_rtc_time.tm_hour = rtc_time.Hours;
 current_rtc_time.tm_min = rtc_time.Minutes;
 current_rtc_time.tm_sec = rtc_time.Seconds;
 current_rtc_time.tm_mday = rtc_date.Date;
 current_rtc_time.tm_mon = rtc_date.Month - 1;
 current_rtc_time.tm_year = rtc_date.Year + 100;
 
 current_rtc_time.tm_isdst = -1;
 
 return (uint32_t)mktime(&current_rtc_time);
}

But sometimes I get wrong time. It should be 0x63xxxxxx in hexadecimal if you convert epoch time but I get 0x78xxxxxx.

This is my RTC init function:

void rtc_init(void)
{
 hrtc.Instance = RTC;
 hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
 hrtc.Init.AsynchPrediv = 127;
 hrtc.Init.SynchPrediv = 255;
 hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
 hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
 hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
 hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
 hrtc.Init.OutPutPullUp = RTC_OUTPUT_PULLUP_NONE;
 APP_ERROR_CHECK (HAL_RTC_Init(&hrtc));
}

This is my MSP Init function:

void HAL_RTC_MspInit(RTC_HandleTypeDef* hrtc)
{
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 if(hrtc->Instance==RTC)
 {
 /** Initializes the peripherals clock
 */
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_RTC;
 PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
 APP_ERROR_CHECK (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit));
 
 /* Peripheral clock enable */
 __HAL_RCC_RTC_ENABLE();
 }
 
}

I am using LSE as the clock source. What could be the issue here?

NOTE: Here is APP_ERROR_CHECK define:

#define APP_ERROR_CHECK(ERR_CODE) \
 do \
 { \
 const uint32_t LOCAL_ERR_CODE = (ERR_CODE); \
 if (LOCAL_ERR_CODE != HAL_OK) 		\
 { \
 	Error_Handler(LOCAL_ERR_CODE, __FILE__, __LINE__); \
 } \
 } while (0)

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
Nov 8, 2022 8:19 AM UTC

When setting time/date, make sure all fields of structs used are cleared or explicitly set.

​

http://www.efton.sk/STM32/gotcha/g113.html

​

JW​

​