Skip to main content
diewet
Visitor II
Sep 19, 2022 8:27 AM UTC
Question

Receiving data with USART in LIN mode using interrupts does not work.

I try to receive data with the USART1 in LIN mode using interrupts. Unfortunately I can't get it to work. This is the configuration of the USART1:

0693W00000Svg5YQAR.png0693W00000Svg5nQAB.png0693W00000Svg6MQAR.pngThe signal on the LIN bus is composed of the LIN break (HAL_LIN_SendBreak(&huart1);), the sync part (HAL_UART_Transmit_IT(&huart1, 0x55, 1);) and an ID (HAL_UART_Transmit_IT(&huart1, 0x0A, 1);).

The signal looks proper on the oscilloscope. While debugging, I can observe that at least the LIN break is detected by the USART1 (LBDF is set). I expected, that at some point the HAL_UART_RxCpltCallback is called, but that never happens.

What am I doing wrong?

main.c:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2022 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "cmsis_os.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "UART_DbgDef.h"
#include "stm32f7xx_ll_usart.h"
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
 
CAN_HandleTypeDef hcan3;
 
CRC_HandleTypeDef hcrc;
 
DMA2D_HandleTypeDef hdma2d;
 
I2C_HandleTypeDef hi2c3;
 
LTDC_HandleTypeDef hltdc;
 
QSPI_HandleTypeDef hqspi;
 
RTC_HandleTypeDef hrtc;
 
SAI_HandleTypeDef hsai_BlockA2;
 
TIM_HandleTypeDef htim4;
TIM_HandleTypeDef htim14;
 
UART_HandleTypeDef huart1;
UART_HandleTypeDef huart6;
 
HCD_HandleTypeDef hhcd_USB_OTG_FS;
 
SDRAM_HandleTypeDef hsdram1;
 
osThreadId defaultTaskHandle;
/* USER CODE BEGIN PV */
 
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void PeriphCommonClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_LTDC_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_CRC_Init(void);
static void MX_DMA2D_Init(void);
static void MX_FMC_Init(void);
static void MX_QUADSPI_Init(void);
static void MX_I2C3_Init(void);
static void MX_SAI2_Init(void);
static void MX_ADC1_Init(void);
static void MX_TIM14_Init(void);
static void MX_RTC_Init(void);
static void MX_CAN3_Init(void);
static void MX_USB_OTG_FS_HCD_Init(void);
static void MX_TIM4_Init(void);
static void MX_USART6_UART_Init(void);
void StartDefaultTask(void const * argument);
 
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
	UART_Debug("HAL_UART_RxCpltCallback");
}
 
void HAL_UART_RxHalfCpltCallback(UART_HandleTypeDef *huart)
{
	UART_Debug("HAL_UART_RxHalfCpltCallback");
}
 
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
{
	UART_Debug("HAL_UART_TxCpltCallback");
}
 
void HAL_UART_TxHalfCpltCallback(UART_HandleTypeDef *huart)
{
	UART_Debug("HAL_UART_TxHalfCpltCallback");
}
/* USER CODE END 0 */
 
/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
/* Configure the peripherals common clocks */
 PeriphCommonClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_LTDC_Init();
 MX_USART1_UART_Init();
 MX_CRC_Init();
 MX_DMA2D_Init();
 MX_FMC_Init();
 MX_QUADSPI_Init();
 MX_I2C3_Init();
 MX_SAI2_Init();
 MX_ADC1_Init();
 MX_TIM14_Init();
 MX_RTC_Init();
 MX_CAN3_Init();
 MX_USB_OTG_FS_HCD_Init();
 MX_TIM4_Init();
 MX_USART6_UART_Init();
 /* USER CODE BEGIN 2 */
 
 /* USER CODE END 2 */
 
 /* USER CODE BEGIN RTOS_MUTEX */
 /* add mutexes, ... */
 /* USER CODE END RTOS_MUTEX */
 
 /* USER CODE BEGIN RTOS_SEMAPHORES */
 /* add semaphores, ... */
 /* USER CODE END RTOS_SEMAPHORES */
 
 /* USER CODE BEGIN RTOS_TIMERS */
 /* start timers, add new ones, ... */
 /* USER CODE END RTOS_TIMERS */
 
 /* USER CODE BEGIN RTOS_QUEUES */
 /* add queues, ... */
 /* USER CODE END RTOS_QUEUES */
 
 /* Create the thread(s) */
 /* definition and creation of defaultTask */
// osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 4096);
// defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
 
 /* USER CODE BEGIN RTOS_THREADS */
 /* add threads, ... */
 /* USER CODE END RTOS_THREADS */
 
 /* Start scheduler */
// osKernelStart();
 
 /* We should never get here as control is now taken by the scheduler */
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 HAL_GPIO_WritePin(LIN__SLP_GPIO_Port, LIN__SLP_Pin, GPIO_PIN_SET);	// Enable external LIN transceiver TJA1027T.
 while (1)
 {
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
	 HAL_Delay(1000);
 }
 /* USER CODE END 3 */
}

This topic has been closed for replies.