Skip to main content
SNish
Associate II
August 18, 2025
Solved

Query about STM32F446 HSE pll setting failure on CubeMX

I am using NucleoF446RE (STM32F446RE) with CubeIDE 1.19.0.
I wish to set PLL  as 16MHz by HSE (STLINK 8MHz MCO).
Because HSI clock is 16MHz.
I had set PLL M/N/P = 4/64/8. 
CubeMX reported P was fail . ]

faiilure PLL.png


So I had set P=4. and It makes PLL-CLK = 32MHz

success pll.png

After hal generation I have modified SystemClock_Config as following.

 

void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct = {0};

RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 

/** Configure the main internal regulator output voltage

*/

__HAL_RCC_PWR_CLK_ENABLE();

__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);

 

/** Initializes the RCC Oscillators according to the specified parameters

* in the RCC_OscInitTypeDef structure.

*/

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

RCC_OscInitStruct.PLL.PLLM = 4;

RCC_OscInitStruct.PLL.PLLN = 64;

RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV8;// Hnad modify

RCC_OscInitStruct.PLL.PLLQ = 2;

RCC_OscInitStruct.PLL.PLLR = 3;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

Error_Handler();

}

 

/** Initializes the CPU, AHB and APB buses clocks

*/

RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)

{

Error_Handler();

}

HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_PLLCLK, RCC_MCODIV_1);

}

 

Code works fine, I cannot see any condition from RM0390 on this point.
Ple

This topic has been closed for replies.
TDK
TDKBest answer
August 18, 2025

Hover over the red area to find an explanation of the issue. In this case:

TDK_0-1755534759184.png

 

Unclear why it wants that. Seems like a bug but I could be missing something.

"If you feel a post has answered your question, please click ""Accept as Solution""."

4 replies

TDK
TDKBest answer
August 18, 2025

Hover over the red area to find an explanation of the issue. In this case:

TDK_0-1755534759184.png

 

Unclear why it wants that. Seems like a bug but I could be missing something.

"If you feel a post has answered your question, please click ""Accept as Solution""."
SNish
SNishAuthor
Associate II
August 18, 2025

Dear TDK 

I am referring on RM0390 (STM32F446xx).
I cannot find out 24MHz limitation on that.
Is it CubeMX message bundled information only ?

regards