PWM output generation from NUCLEO-F031K6 (MCU: STM32F031K6) is not working. Code is generated from STM32CubeMx.
I'm using NUCLEO-F031K6 (MCU: STM32F031K6) for PWM output generation (100Hz clock). Project is generated from STM32CubeMx v5.6.1.
PA11 (TIM1_CH4) is used for PWM output. No clock pulses are seen.
APB1 timer clock is 8MHz.
------------------------------------
Timer-1 settings:-
------------------------------------
Prescaler: 79
Counter Period: 999
Pulse: 500
Any clue?
GPIO toggle is working for the same pin, PA11