Skip to main content
malcolm23
Associate II
Nov 5, 2018 10:09 PM UTC
Question

Putting STM32F7xx_HAL_Driver and FreeRTOS in Library does not work

I have an IAR example STM32F746 project which brings up an LwIP stack on top of FreeRTOS; however I'm trying to turn it into a library and link into around 10-15 applications. This is breaking badly because linking via libraries doesn't appear to obey the __weak attribute.

The STM32F7xx_HAL_Driver uses __weak to expose symbols it allows the user to override, e.g:

__weak void HAL_MspInit(void)

I have an override of this in my application code (the auto-generated stm32f7xx_hal_msp.c file). When compiled as an application, the linker selects my version over the __weak version. When compiled as a library and then linked into an empty application, the linker selects the __weak version.

The only workaround I have found is to comment out the __weak versions of the functions when they have been overridden and my program works again.

Do you have any better suggestions than commenting out chunks of the HAL_Driver library?

---- UPDATE ---

I found a different solution which I believe works better than the current __weak approach. The __weak actually has two meanings:

  1. A __weak symbol may have multiple definitions, and strong definitions override weak
  2. __weak symbols may optionally not be defined, and will have a null address if undefined.

The HAL_Driver library is attempting to use __weak in its first meaning where the user provided function overrides the default implementation. Instead the second approach works better. For example the declaration of HAL_MspInit should be:

__weak void HAL_MspInit(void);

Then its call in HAL_Init() should be replaced with:

/* Init the low level hardware */

if (HAL_MspInit)

HAL_MspInit();

Not only does this approach work for libraries, but this has the potential to be more efficient than the current approach in that the compiler has a chance of totally optimizing the call out for functions not implemented by the user.

There are something like 270 __weak functions in the STM32F7xx HAL_Driver library, and some of them actually do work if not overridden by the user (they need an else to the if in the example above). Food for thought!

This topic has been closed for replies.

1 reply

ADunc.1
Senior
Apr 30, 2020 11:06 PM UTC

I know this answer is much too late...

The usual cause of this in my experience, is due to the linker discarding the stm32xxxx_hal_msp.c file completely as there are no direct calls into that file. It thinks nothing calls those functions so they are unused. For example if you added a function into the stm32xxxx_hal_msp.c file and called it from another file, then the stm32xxxx_hal_msp.c file will not be discarded during linking and the weak functions will be overridden by the ones in stm32xxxx_hal_msp.c.

There are linker flags to prevent discarding unused sections, but they cause it to keep ALL unused sections.

This applies for sure with GCC but I don't know about IAR.