Skip to main content
IBely.3
Associate
August 13, 2019
Question

Problem with packages in STM32Cube

Hello, I can't download none of packages in STM32CubeMX. There is error with message ".... not available...".  

Trying to install manually causes error message "...Problem During Unzip File....". 

Trying to set the path to Firmware location manually in project manager causes error message "...The selected firmware should contain at least Drivers\STM32L1xx_HAL_Driver and Driver\CMSIS Folders". The folder with firmware was downloaded from official site. 

What s wrong with my STM32CubeMX?

This topic has been closed for replies.

8 replies

Tesla DeLorean
Guru
August 13, 2019

Make sure you have enough free space on the disk being used for the repository. Some of the 1GB downloads will need 3GB of free space.

By default I think ST sets it in a user directory, but I've tended to park it elsewhere.

Use the "Test" functionality within WinRar or equivalent tools, to validate the .ZIP file integrity.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
IBely.3
IBely.3Author
Associate
October 28, 2019

Sorry, but what you mean when you say "Test" functionality?

IBely.3
IBely.3Author
Associate
October 28, 2019

Sorry, but what you mean when you say "Test" functionality?

Tesla DeLorean
Guru
October 28, 2019

WinRar provides a means to test the integrity of the archive without actually unpacking it on your hard drive.

0690X00000ArMv0QAF.jpg

You can also download the CubeL1 package more directly, and "Install from Local"

Make sure you have sufficient disk space, and you don't have AV or firewall software interfering with your ability to download and unpack archives.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
IBely.3
IBely.3Author
Associate
October 29, 2019

Solution was very simple... Help->Updater Settings->->Updater Settings->Repository Folder, my path contains cyrillic letters, after changing the path, everything worked OK.

Tesla DeLorean
Guru
October 29, 2019

That stuff is probably not well tested. Things in Windows using cyrillic or pictographs, spaces, etc can cause problems. Desktop and Program File "directories" can also be a problem.

ST also wants to put the repository, including packed and unpacked files, into a "Per User" directory, this seems a bit crazy when a lot of the archives are 1GB and total unpack/packed footprint pushes 3-4GB. Places with sharper knives in the draw would leave the stuff in the ZIP file, and create a ZIP-FS to pull out the specific files of interests when duping more of this stuff into additional user project directories at every invocation.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Sergei Kolesnik
Visitor II
June 6, 2020

Same problem:

Error was "Problem during unzip file"

One of the simple solution: Run CubeMX with administrator rights!!!11

#STM32CubeF1 problem during unzip file

Aeae.1
Visitor II
January 5, 2021

These are a chunk like Butter Knives, I use gadgets which can be loads sharper, which I fashioned myself. The use of easier/prolific equipment has a tendency to be improved appreciably with publish-processing here to reformat to a favored fashion with glide and interplay paths diagnosed.