Skip to main content
Maciej Frankowski
Associate
March 26, 2024
Question

Problem with LD files in CubeMX (6.11.0) & CubeIDE (1.15.0)

Hi,

I use several LD files in the project, depending on the selected build. After updating CubeMX (6.11.0) and CubeIDE (1.15.0), the default LD file appears in the project every time I generate code from CubeMX. Worst of all, all links to my LD files are removed. Each time I have to laboriously edit the project settings. Nightmare. Do you have that too?

Regards.

This topic has been closed for replies.

3 replies

Ghofrane GSOURI
ST Technical Moderator
April 1, 2024

Hello @Maciej Frankowski 

I would appreciate it if you could give me the project where you encountered the issue or at least provide me with the steps that I need to follow to reproduce it.

Also is this issue consistently reproduced?

I will be waiting for your feedback.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Ghofrane GSOURI
ST Technical Moderator
April 3, 2024

Hello again @Maciej Frankowski 

Thank you for your contributions and for your detailed explanations,

I confirm the issue on my side, it has been reported to STM32CubeMX development team .

Internal ticket number: 178127  (This is an internal tracking number and is not accessible or usable by customers).

I will keep you posted with updates.

 

Regards,

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Maciej Frankowski
Associate
April 3, 2024
Hi Ghofrane,
Two things.
 
First, generating code with CubeMX places default file, e.g. STM32L071KBTX_FLASH.ld, in the project directory. I understand that. But why does this happen every time? You can delete this file and it reappears anyway.
 
Secondly, the reference to my modified file, e.g. STM32L071KBTX_FLASH_DEBUG.ld, is replaced with the default name:
Properties -> C/C++ Build -> Settings -> Tool Settings -> MCU GCC Linker -> General -> Linker Script (-T) -> (...)STM32L071KBTX_FLASH.ld
In the previous version of the environment, this did not happen. I have several configurations, and they all fail.
 
Best Regards
Maciej