Skip to main content
giver3
Associate
Jan 12, 2015 10:38 AM UTC
Question

Problem with CubeMX 4.5.0 with Linux

Posted on January 12, 2015 at 11:38

Hello all.

Bed path:

java.io.FileNotFoundException: /home/krzysiek/STMicroelectronics/STM32Cube/STM32CubeMX/db/plugins/projectmanager\stm32tck.cfg (No such file or directory)

at java.io.FileInputStream.open(Native Method)

at java.io.FileInputStream.<init>(FileInputStream.java:146)

at java.io.FileInputStream.<init>(FileInputStream.java:101)

at java.io.FileReader.<init>(FileReader.java:58)

at convertor.Convertor.getTplVer(Convertor.java:1152)

at convertor.Convertor.setTemplates(Convertor.java:536)

at convertor.Convertor.setDataPath(Convertor.java:1495)

at com.st.microxplorer.plugins.projectmanager.model.ToolchainGenerator.setDllDataPath(ToolchainGenerator.java:116)

at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createToolChainFolders(ProjectBuilder.java:934)

at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:339)

at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:36)

Project Generator version: 1.5.1

[Project Generator] Problem in the project generation

java.io.FileNotFoundException: /home/krzysiek/STMicroelectronics/STM32Cube/STM32CubeMX/db/plugins/projectmanager\stm32tck.cfg (No such file or directory)

at java.io.FileInputStream.open(Native Method)

at java.io.FileInputStream.<init>(FileInputStream.java:146)

at java.io.FileInputStream.<init>(FileInputStream.java:101)

at java.io.FileReader.<init>(FileReader.java:58)

at convertor.Convertor.getTplVer(Convertor.java:1152)

at convertor.Convertor.setTemplates(Convertor.java:536)

at convertor.Convertor.convert(Convertor.java:377)

at convertor.Convertor.generate(Convertor.java:1476)

at com.st.microxplorer.plugins.projectmanager.model.ToolchainGenerator.generate(ToolchainGenerator.java:53)

at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createToolChainFolders(ProjectBuilder.java:948)

at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:339)

at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:36)

mx.scratch is deleted!

Time for Generating toolchain IDE Files: 9mS.

Error in Project Generation

#linux #cubemx
This topic has been closed for replies.

2 replies

Martin Davey
Associate III
Feb 16, 2015 1:56 PM UTC
Posted on February 16, 2015 at 14:56

Hi,

I think you will find it targets windows only at the moment. However, if you look at this project: http://www.openstm32.org

It sounds like there will have to be a linux version fairly soon?

Marty.

stm32cube-t
ST Employee
Feb 9, 2016 11:16 AM UTC
Posted on February 09, 2016 at 12:16

Dear user,

This issue is now fixed.